| module ti.uia.events.UIASync |
 |
 |
 |
UIA Synchronization Events
The UIASync module defines events that enable
correlation of events from multiple cores as well as
correlation of software events with hardware trace
[
more ... ]
#include <ti/uia/events/UIASync.h>
Functions common to all target modules |
|
|
Constants |
| |
| |
| |
| |
DETAILS
The UIASync module defines events that enable
correlation of events from multiple cores as well as
correlation of software events with hardware trace
The following configuration script demonstrates how to configure an
application to log sync point events, using the default configuration
settings provided by the LogSync module. By default, the LogSync module
creates a dedicated 256 byte LoggerCircBuf logger to use to capture
sync point events. By default, the Rta module logs sync point events
when it receives a start or stop command, or before sending up an
event packet if the LogSync.isSyncPointRequired API returns 'true'.
SEE
EXAMPLES
Example 1: This is part of the XDC configuration file for the application:
// the LogSync module internally does xdc.useModule('ti.uia.events.UIASync')
var LogSync = xdc.useModule('ti.uia.runtime.LogSync');
var Rta = xdc.useModule('ti.uia.services.Rta');
| config UIASync_globalTimerFreq // module-wide |
 |
syncPoint event containing global timer frequency information
extern const Log_Event UIASync_globalTimerFreq;
VALUES
serialNumber
a 32b serial number, used for correlation with HW
trace sync points
CpuCyclesPerGlobalTimerTick
the number of CPU cycles per global
timer increment. 0 if no conversion possible.
GlobalTimerFreqLSW
the 32 LSBs of the Global Timer frequency
GlobalTimerFreqMSW
the 32 MSBs of the Global Timer frequency
DETAILS
This event logs clock information that allows the host to determine how
to convert global imestamp tick counts into time values and CPU cycle
counts.
| config UIASync_syncPoint // module-wide |
 |
syncPoint event
VALUES
serialNumber
a 32b serial number, used for correlation with HW
trace sync points
CpuTimestampLSW
the 32 LSBs of the global timestamp
CpuTimestampMSW
the 32 MSBs of the global timestamp
GlobalTimestampLSW
the 32 LSBs of the global timestamp
GlobalTimestampMSW
the 32 MSBs of the global timestamp
CpuCyclesPerCpuTimerTick
the number of CPU cycles per CPU timer
increment. 0 if no conversion possible.
CPUFreqLSW
the 32 LSBs of the CPU frequency
CPUFreqMSW
the 32 MSBs of the CPU frequency
DETAILS
This event logs both a local CPU timestamp (the event timestamp) and a
global timestamp, which enables time correlation of the
local CPU timestamps that each event can be tagged with
against the global timebase, thus enabling multi-core
event correlation. It also logs clock information that allows the host
to determine how to convert CPU timestamp tick counts into time values
and CPU cycle counts.
| config UIASync_syncPointAfterHalt // module-wide |
 |
syncPoint event logged after the CPU has resumed running after being
reset, suspended or halted by the debugger
extern const Log_Event UIASync_syncPointAfterHalt;
VALUES
serialNumber
a 32b serial number, used for correlation with HW
trace sync points
CpuTimestampLSW
the 32 LSBs of the global timestamp
CpuTimestampMSW
the 32 MSBs of the global timestamp
GlobalTimestampLSW
the 32 LSBs of the global timestamp
GlobalTimestampMSW
the 32 MSBs of the global timestamp
CpuCyclesPerCpuTimerTick
the number of CPU cycles per CPU timer
increment. 0 if no conversion possible.
CPUFreqLSW
the 32 LSBs of the CPU frequency
CPUFreqMSW
the 32 MSBs of the CPU frequency
DETAILS
This event logs both a local CPU timestamp (the event timestamp) and a
global timestamp, which enables time correlation of the
local CPU timestamps that each event can be tagged with
against the global timebase, thus enabling multi-core
event correlation. It also logs clock information that allows the host
to determine how to convert CPU timestamp tick counts into time values
and CPU cycle counts.
| config UIASync_syncPointUserProvidedData // module-wide |
 |
An event that provides supplementary info to a sync point event
extern const Log_Event UIASync_syncPointUserProvidedData;
VALUES
serialNumber
a 32b serial number, used for correlation with
HW trace sync points
fmt
a format specifier string for up to 6 additional parameters
DETAILS
This event can be used by user-provided code to log supplementary
event data whenever a sync point event is logged.
| Module-Wide Built-Ins |
 |
// Get this module's unique id
Bool UIASync_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool UIASync_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 UIASync_Module_getMask();
// Returns the diagnostics mask for this module
Void UIASync_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
var UIASync = xdc.useModule('ti.uia.events.UIASync');
module-wide config parameters
msg: "Sync Point Global Timer Freq: SerialNumber=0x%x, CpuCyclesPerGlobalTimerTick=%d, GlobalTimerFreq [LSW=0x%x, MSW=0x%x]"
};
msg: "Sync Point: SerialNumber=0x%x, CpuTStamp [LSW=0x%x, MSW=0x%x], GlobalTStamp [LSW=0x%x, MSW=0x%x], CpuCyclesPerCpuTimerTick=%d, CpuFreq [LSW=0x%x, MSW=0x%x]"
};
msg: "Sync Point After Halt: SerialNumber=0x%x, CpuTStamp [LSW=0x%x, MSW=0x%x], GlobalTStamp [LSW=0x%x, MSW=0x%x], CpuCyclesPerCpuTimerTick=%d, CpuFreq [LSW=0x%x, MSW=0x%x]"
};
msg: "Sync Point User Data: SerialNumber=0x%x, %$S"
};
| config UIASync.globalTimerFreq // module-wide |
 |
syncPoint event containing global timer frequency information
msg: "Sync Point Global Timer Freq: SerialNumber=0x%x, CpuCyclesPerGlobalTimerTick=%d, GlobalTimerFreq [LSW=0x%x, MSW=0x%x]"
};
VALUES
serialNumber
a 32b serial number, used for correlation with HW
trace sync points
CpuCyclesPerGlobalTimerTick
the number of CPU cycles per global
timer increment. 0 if no conversion possible.
GlobalTimerFreqLSW
the 32 LSBs of the Global Timer frequency
GlobalTimerFreqMSW
the 32 MSBs of the Global Timer frequency
DETAILS
This event logs clock information that allows the host to determine how
to convert global imestamp tick counts into time values and CPU cycle
counts.
C SYNOPSIS
| config UIASync.syncPoint // module-wide |
 |
syncPoint event
msg: "Sync Point: SerialNumber=0x%x, CpuTStamp [LSW=0x%x, MSW=0x%x], GlobalTStamp [LSW=0x%x, MSW=0x%x], CpuCyclesPerCpuTimerTick=%d, CpuFreq [LSW=0x%x, MSW=0x%x]"
};
VALUES
serialNumber
a 32b serial number, used for correlation with HW
trace sync points
CpuTimestampLSW
the 32 LSBs of the global timestamp
CpuTimestampMSW
the 32 MSBs of the global timestamp
GlobalTimestampLSW
the 32 LSBs of the global timestamp
GlobalTimestampMSW
the 32 MSBs of the global timestamp
CpuCyclesPerCpuTimerTick
the number of CPU cycles per CPU timer
increment. 0 if no conversion possible.
CPUFreqLSW
the 32 LSBs of the CPU frequency
CPUFreqMSW
the 32 MSBs of the CPU frequency
DETAILS
This event logs both a local CPU timestamp (the event timestamp) and a
global timestamp, which enables time correlation of the
local CPU timestamps that each event can be tagged with
against the global timebase, thus enabling multi-core
event correlation. It also logs clock information that allows the host
to determine how to convert CPU timestamp tick counts into time values
and CPU cycle counts.
C SYNOPSIS
| config UIASync.syncPointAfterHalt // module-wide |
 |
syncPoint event logged after the CPU has resumed running after being
reset, suspended or halted by the debugger
msg: "Sync Point After Halt: SerialNumber=0x%x, CpuTStamp [LSW=0x%x, MSW=0x%x], GlobalTStamp [LSW=0x%x, MSW=0x%x], CpuCyclesPerCpuTimerTick=%d, CpuFreq [LSW=0x%x, MSW=0x%x]"
};
VALUES
serialNumber
a 32b serial number, used for correlation with HW
trace sync points
CpuTimestampLSW
the 32 LSBs of the global timestamp
CpuTimestampMSW
the 32 MSBs of the global timestamp
GlobalTimestampLSW
the 32 LSBs of the global timestamp
GlobalTimestampMSW
the 32 MSBs of the global timestamp
CpuCyclesPerCpuTimerTick
the number of CPU cycles per CPU timer
increment. 0 if no conversion possible.
CPUFreqLSW
the 32 LSBs of the CPU frequency
CPUFreqMSW
the 32 MSBs of the CPU frequency
DETAILS
This event logs both a local CPU timestamp (the event timestamp) and a
global timestamp, which enables time correlation of the
local CPU timestamps that each event can be tagged with
against the global timebase, thus enabling multi-core
event correlation. It also logs clock information that allows the host
to determine how to convert CPU timestamp tick counts into time values
and CPU cycle counts.
C SYNOPSIS
| config UIASync.syncPointUserProvidedData // module-wide |
 |
An event that provides supplementary info to a sync point event
msg: "Sync Point User Data: SerialNumber=0x%x, %$S"
};
VALUES
serialNumber
a 32b serial number, used for correlation with
HW trace sync points
fmt
a format specifier string for up to 6 additional parameters
DETAILS
This event can be used by user-provided code to log supplementary
event data whenever a sync point event is logged.
C SYNOPSIS
| metaonly config UIASync.common$ // module-wide |
 |
Common module configuration parameters
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
generated on Wed, 16 May 2018 18:08:35 GMT