| config Main.usage // module-wide |
 |
Usage for this command
| XDCscript usage |
meta-domain |
Main.usage = String[] [
' ',
'Usage',
'[-p] [-h] [-m] [-e executable] [-x RTA XML file] [-o output text file] [-c delimter character]',
'[--help]',
' '
];
| Main.exec() // module-wide |
 |
'xs' script entry point
| XDCscript usage |
meta-domain |
Main.exec(Any args) returns Any
| Main.main() // module-wide |
 |
'xs' shell entry point
| XDCscript usage |
meta-domain |
Main.main(Any args) returns Any
| Instance Config Parameters |
 |
| XDCscript usage |
meta-domain |
var params = new Main.Params;
// Instance config-params object
params.delimiter = String "|";
// // TODO
[-l output file for load data]
params.executable = String "";
// Path to the executable which was used to generate the data file
params.more = Bool false;
// Wait for the user to press enter before displaying the next packet
params.outputFile = String "";
// Optional path to an output file to write the decoded records to
params.printToScreen = Bool false;
// Whether to print the decoded records to the console
params.rtaXml = String "";
// Optional path to the RTA XML file
params.suppressHeader = Bool false;
// Don't print the header when printing the decoded records
| config Main.delimiter // instance |
 |
// TODO
[-l output file for load data]
| XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.delimiter = String "|";
DETAILS
Delimiter character to use when writing out the file.
The character specified here will be inserted between each of the
record fields so that the file can be imported into a spreadsheet
such as excel.
| config Main.executable // instance |
 |
Path to the executable which was used to generate the data file
| XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.executable = String "";
| config Main.more // instance |
 |
Wait for the user to press enter before displaying the next packet
| XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.more = Bool false;
DETAILS
Without this flag, the tool will simply print all of the records in the
data file to the screen. If this flag is set, then the tool will wait
the user to press enter in between displaying each packet.
| config Main.outputFile // instance |
 |
Optional path to an output file to write the decoded records to
| XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.outputFile = String "";
DETAILS
The tool will write the decoded records out as text to the specified
out file. The record properties will be separated with a delimeter
character so that they can be imported into a spreadsheet such as
Excel.
| config Main.printToScreen // instance |
 |
Whether to print the decoded records to the console
| XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.printToScreen = Bool false;
DETAILS
You may use this tool to simply print the decoded records, or you
may have them redirected to a file to be processed elsewhere.
| config Main.rtaXml // instance |
 |
Optional path to the RTA XML file
| XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.rtaXml = String "";
| config Main.suppressHeader // instance |
 |
Don't print the header when printing the decoded records
| XDCscript usage |
meta-domain |
var params = new Main.Params;
...
params.suppressHeader = Bool false;
| Main.run() // instance |
 |
Underlying implementation
| XDCscript usage |
meta-domain |