| module ti.uia.runtime.Transport |
 |
 |
 |
Transport function specification module
This module defines the function prototypes for the transport functions
that can be plugged into the ServiceMgr. UIA ships several
implementations of this interface in the ti/uia/sysbios directory.
[
more ... ]
#include <ti/uia/runtime/Transport.h>
Functions common to all target modules |
|
|
Typedefs |
typedef struct | |
DETAILS
This module defines the function prototypes for the transport functions
that can be plugged into the ServiceMgr. UIA ships several
implementations of this interface in the ti/uia/sysbios directory.
The implementations do not have to be XDC modules. They are simply standard
'C' functions (i.e look at ti/uia/sysbios/TransportNdk.c). Only one
transport set can be used on a target and it needs to be set up at build
time via the
ti.uia.runtime.ServiceMgr.transportFxns parameter. The
ServiceMgr plugs the transportFxns automatically based on the TransportType
ti.uia.runtime.ServiceMgr.transportType.
If someone writes an new transport
(e.g. RapidIO), they can be plugged in by setting the TransportType
to
ti.uia.runtime.ServiceMgr.TransportType_USER and then plugging
the transportFxns manually. It must also set up the following parameters
as directed by the new transport developer.
- ServiceMgr.supportControl: does the transport support receiving messages
from the host. For example TransportFile does not.
- ServiceMgr.maxEventPacketSize: Max size of an outgoing event packet. For
example TransportNdk uses 1472 (emac size minus headers)
- ServiceMgr.maxCtrlPacketSize: Max size of the message packets. This can
be zero if supportControl is false.
Here is an example of plugging the transport XYZ into the ServiceMgr:
var ServiceMgr = xdc.useModule('ti.uia.runtime.ServiceMgr');
ServiceMgr.transportType = ServiceMgr.TransportType_USER;
var xyzTransport = {
initFxn: '&TransportXYZ_init',
startFxn: '&TransportXYZ_start',
recvFxn: '&TransportXYZ_recv',
sendFxn: '&TransportXYZ_send',
stopFxn: '&TransportXYZ_stop',
exitFxn: '&TransportXYZ_exit',
};
ServiceMgr.transportFxns = xyzTransport;
ServiceMgr.maxEventPacketSize = 1024
ServiceMgr.maxCtrlPacketSize = 1024;
ServiceMgr.supportControl = true;
TRANSPORT FUNCTIONS
The following are the transport functions. Note
all of these functions
are called by the ServiceMgr. The application should not be calling
these functions directly.
- initFxn: Called during module startup (which is before main()). Minimal
actions can take place here since there are no interrupts and
the state of the application is just starting up. Generally only
internal initialization is done in this function.
- startFxn: The start function is called at once or twice after the SYS/BIOS
tasks have started to run. The start
function is called with UIAPacket_HdrType_EventPkt before any
events are sent. This allows the transport to initialize
anything needed for event transmission. The function returns a
handle to a transport specific structure (or NULL if not needed).
This handle is passed into the sendFxn and stopFxn.
If the transport supports control messages from a host, the
start function is called with UIAPacket_HdrType_Msg.
This allows the transport to initialize anything needed for
msg transmission (both sending and receiving). Again, the
transport can return a transport specific structure. This
structure can be different from the one returned in the
UIAPacket_HdrType_EventPkt start.
- recvFxn: The recv function is called to receive incoming messages
from the host. The handle returned from the start is passed
into the recv. Also passed in is a buffer and its size.
The buffer is passed in as a double pointer. This allows
the transport to double-buffer. For example, the recv
function can return a different buffer than what was
passed in. This potentially reduces extra copies of the data.
The recv can be a blocking call.
The recv returns the actual number of bytes that are placed into
the buffer. If the transport does not
support control messages, this function can simply return zero.
- sendFxn: The send function is called to send either events or msgs. If
send is called to transmit a event, the first parameter is the
handle returned from the start(UIAPacket_HdrType_EventPkt).
Similiarily, if a message is being sent, the first parameter is
the handle returned from the start(UIAPacket_HdrType_Msg).
The size of the packet is maintained in the UIAPacket_Hdr.
The send can be a blocking call.
This function returns whether the send was successful or not.
Again a double pointer is used to allow the transport to return
a different buffer to allow double-buffering.
- stopFxn: The stop function is to counterpart to the start function. The
stop will be called the same number of times as the start. The
calls will contain handles returned from the start.
- exitFxn: The exit function is to counterpart to the init function.
Transport are allowed to have additional functions that can be directly
called by the application. For example in ti/uia/sysbiosTransportFile,
there is a TransportFile_setFile function. The downside to the extended
functions is portability.
| struct Transport_FxnSet |
 |
Task hook set type definition
typedef struct Transport_FxnSet {
Void (*initFxn)();
Void (*stopFxn)(Ptr);
Void (*exitFxn)(Void);
} Transport_FxnSet;
DETAILS
| Module-Wide Built-Ins |
 |
// Get this module's unique id
Bool Transport_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool Transport_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 Transport_Module_getMask();
// Returns the diagnostics mask for this module
Void Transport_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
var Transport = xdc.useModule('ti.uia.runtime.Transport');
module-wide constants & types
module-wide config parameters
generated on Wed, 26 Oct 2011 00:41:36 GMT