| module ti.uia.runtime.LogSync |
 |
 |
 |
SyncPoint Event logging module for logging sync point events. Allows sync
point events to use a different logger instance than used for other events
SyncPoint events are used to log timestamp values for two timebases: the
local CPU timestamp that is used to timestamp events from this CPU, and a
'global' timestamp value that can be accessed by two or more CPUs.
By logging the current timestamp values from these two timebase sources,
the sync point events provide correlation points between the two timebases.
[
more ... ]
#include <ti/uia/runtime/LogSync.h>
Functions |
Bool | |
Bool | |
Bool | |
Void | |
Void | |
macro Void | |
Functions common to all target instances |
|
LogSync_handle// Convert this instance structure pointer into an instance handle,
LogSync_Handle_label// The label associated with this instance object,
LogSync_Handle_name// The name of this instance object,
LogSync_Object_count// The number of statically-created instance objects,
LogSync_Object_first// The handle of the first dynamically-created instance object, or NULL,
LogSync_Object_get// The handle of the i-th statically-created instance object (array == NULL),
LogSync_Object_heap// The heap used to allocate dynamically-created instance objects,
LogSync_Object_next// The handle of the next dynamically-created instance object, or NULL,
LogSync_struct// Convert this instance handle into an instance structure pointer
|
Functions common to all target modules |
|
|
Typedefs |
| |
typedef struct | |
typedef struct | |
typedef struct | |
Constants |
extern const UInt32 | |
extern const UInt32 | |
| |
| |
DETAILS
SyncPoint events are used to log timestamp values for two timebases: the
local CPU timestamp that is used to timestamp events from this CPU, and a
'global' timestamp value that can be accessed by two or more CPUs.
By logging the current timestamp values from these two timebase sources,
the sync point events provide correlation points between the two timebases.
In order to allow sync point information to be injected into hardware trace
streams, the LogSync module supports a configuration parameter named
injectIntoTraceFxn that allows the user to hook in a function pointer
to a function that handles the (ISA specific) details of injecting whatever
information is required into the trace stream. For C64X+ full gem devices,
the address of the ti.uia.family.c64p.GemTraceSync module's
GemTraceSync_injectIntoTrace function should be used.
The sync point events are defined in the ti.uia.events.UIASync module
(@see ti.uia.events.UIASync#syncPoint)
A unique 'serial number' is assigned to each sync point event that is logged.
The same serial number is logged as a parameter for all UIASync events that are
used to log information related to the sync point, allowing host-side tooling to
treat these separate events coherently. The serial number can optionally be injected
into device-specific trace streams (e.g. CPU trace, System Trace, etc.) in order
to enable host-side tooling to correlate these separate streams with the CPU and
global timestamp information logged with the sync point events.
EXAMPLES
Example 1: This is part of the XDC configuration file for the application
that demonstrates a standard configuration using default settings. In this
example, the Rta module internally handles the logging of the sync point
events. A timestamp module that implements the IUIATimestampProvider
interface is used for the global timestamp. Default values are used for
the CPU maxCpuClockFreq (700 MHz).
// By including Rta, Log records will be collected and sent to the
// instrumentation host (once it is connected and started). The Rta module
// logs sync point events upon receiving either the start or stop command,
// and prior to sending up a new event packet if
// LogSync_isSyncPointEventRequired() returns true.
var Rta = xdc.useModule('ti.uia.services.Rta');
// By default, the sync point events will be logged to a dedicated
// LoggerCircBuf buffer named 'SyncLog' that is assigned to the LogSync
// module. Using a dedicated event logger buffer is recommended
// in order to ensure that sufficient timing information
// is captured to enable accurate multicore event correlation.
// Configure LogSync.defaultSyncLoggerSize to specify a custom buffer size.
var LogSync = xdc.useModule('ti.uia.runtime.LogSync');
// For C64X+ and C66X devices that provide CPU trace hardware capabilities,
// the following line will enable injection of correlation information into
// the GEM CPU trace, enabling correlation of software events with the CPU
// trace events.
var GemTraceSync = xdc.useModule('ti.uia.family.c64p.GemTraceSync');
// Configure a shared timer to act as a global time reference to enable
// multicore correlation. The TimestampC6472Timer module implements the
// IUIATimestampProvider interface, so assigning this timer to
// LogSync.GlobalTimestampProxy will configure the LogSync module's global
// clock parameters automatically. Exmaple 2 shows how to use other
// types of timers.
var TimestampC6472Timer =
xdc.useModule('ti.uia.family.c64p.TimestampC6472Timer');
LogSync.GlobalTimestampProxy = TimestampC6472Timer;
Example 2: Using a timer that does not implement the IUIATimestampProvider
interface as the global timestamp timer. This example shows how to use,
for example, timers that are provided by DSP/BIOS as the global timer
source for event correlation 'sync point' timestamps.
var LogSync = xdc.useModule('ti.uia.runtime.LogSync');
var BiosTimer = xdc.useModule('ti.sysbios.family.c64p.TimestampProvider');
LogSync.GlobalTimestampProxy = BiosTimer;
// The following additional configuration code is required to use
// a timer that does not implement the IUIATimeestampProvider interface
// as the global timer for the LogSync module. If the maxGlobalClockFreq
// config option is not initialized, the following warning message will be displayed
// at build time: "Warning: UIA Event correlation disabled. Please
// configure LogSync.globalClkFreq (.lo,.hi) to a non-zero value to enable."
LogSync.maxGlobalClockFreq.lo = 700000000; // frequency in Hz - lower 32b
LogSync.maxGlobalClockFreq.hi = 0; // frequency in Hz - upper 32b
// Configure the LogSync module with CPU timestamp clock frequency info
// for clock frequencies other than the default (700MHz).
LogSync.maxCpuClockFreq.lo = 1000000000; // 1GHz CPU freq. - lower 32b
LogSync.maxCpuClockFreq.hi = 0; // 1GHz CPU freq.- upper 32b
// The globalTimestampCpuCyclesPerTick config option is optional.
// It is used to convert global timestamp tick counts into CPU cycle counts
// for devices where there is a fixed relationship between the global timer
// frequency and the CPU clock.
LogSync.globalTimestampCpuCyclesPerTick = 6;
Example 3: Disabling LogSync module at configuation time
The logging of sync point events can be disabled by adding the following
to the configuration script:
LogSync.isEnabled = false;
Example 4: This is a part of the C code for an application that does
not use the Rta module, and so needs to log the sync point events itself:
#include <ti/uia/runtime/LogSync.h>
...
// If the target has been suspended or halted
// since the last time an event packet was sent to the
// host, or the event transport has received a 'start' or
// 'stop' command from the host, log a new sync point event to record
// the current correlation info between the local
// timestamp and the global timestamp.
if ((LogSync_isSyncEventRequired())||([starting/stopping event transport])){
LogSync_writeSyncPoint();
}
| config LogSync_cpuTimestampCyclesPerTick // module-wide |
 |
The number of CPU cycles each tick of the global timestamp corresponds to.
0 if no relation between clocks
extern const UInt32 LogSync_cpuTimestampCyclesPerTick;
DETAILS
If the module configured as the CpuTimestampProxy implements
ti.uia.runtime.IUIATimestampProvider, the default value of this config
option is derived at configuration time from that module's config data.
Otherwise it is initialized to 0 to signify that there is no way to
convert a number of global timestamp tick counts into an equivalent
number of CPU cycles.
| config LogSync_globalTimestampCpuCyclesPerTick // module-wide |
 |
The number of CPU cycles each tick of the global timestamp corresponds
to. 0 if no relation between clocks
extern const UInt32 LogSync_globalTimestampCpuCyclesPerTick;
DETAILS
A value of 0 signifies that there is no way to convert a number of
global timestamp tick counts into an equivalent number of CPU cycles.
Note that this value will be automatically copied from the
GlobalTimestampProxy.cpuCyclesPerTick configuration value
at configuration time if GlobalTimestampProxy.cpuCyclesPerTick > 0.
| config LogSync_injectIntoTraceFxn // module-wide |
 |
Callback function that handles injection of info such as serial numbers
of sync point events, context change events or snapshot events into a
hardware trace stream. (e.g. GEM CPU Trace, System Trace, etc.)
DETAILS
Users can provide their own custom injectIntoTraceFxn to log whatever
additional information they wish to record when the hook function is called.
For example, event serial numbers can be injected into the CPU
trace stream and / or STM trace stream in order to enable correlation
of information logged in these streams with UIA software events.
EXAMPLES
Example 1: Correlating events with C64X+ and C66 CPU Trace
The following is an example of the configuration script used
to inject serial numbers of sync point events or context change events or
snapshot Ids associated with snapshot events.
Note that the GemTraceSync module's .xs script takes care of finding
all modules that implement the IUIATraceSyncClient and assigning the
GemTraceSync_injectIntoTrace function pointer to those modules'
injectIntoTraceFxn config option.
//The following 3 modules all implement the IUIATraceSyncClient interface
var LogSnapshot = xdc.useModule('ti.uia.runtime.LogSnapshot');
var LogCtxChg = xdc.useModule('ti.uia.runtime.LogCtxChg');
var LogSync = xdc.useModule('ti.uia.runtime.LogSync');
//For C66 devices, replace the following line with
// var GemTraceSync = xdc.useModule('ti.uia.family.c66.GemTraceSync');
var GemTraceSync = xdc.useModule('ti.uia.family.c64p.GemTraceSync');
Example 2: How to create a custom hook function
and assign it to the LogSnapshot module
The following is an example of a 'C' code program that implements
a hook function that prints out the snapshot ID that is passed in
as the serialNumber
#include <xdc/std.h>
#include <xdc/runtime/Gate.h>
#include <ti/uia/runtime/IUIATraceSyncProvider.h>
#include <ti/uia/runtime/LogSnapshot.h>
#include <stdio.h>
#include <string.h>
extern Void myHookFxn(UInt32 serialNumber, IUIATraceSyncProvider_ContextType ctxType);
Void Test();
char name[32]={"Bob"};
UInt32 newAppId = 0;
Void myHookFxn(UInt32 serialNumber, IUIATraceSyncProvider_ContextType ctxType){
volatile UInt32 syncWord;
IArg key = Gate_enterSystem();
printf("newAppId written with serialNumber %d and ctxType = %d\n",serialNumber,ctxType);
Gate_leaveSystem(key);
}
Void Test(){
// note that the hook function is triggered by calling LogSnapshot_getSnapshotId()
// since that is where the unique snapshot ID that is passed to the
// hook function is generated.
Int snapshotId = LogSnapshot_getSnapshotId();
LogSnapshot_writeString(snapshotId,"User-defined name=%s.",name, strlen(name));
}
Void main(){
while(TRUE){ Test(); }
}
In order to have the above user-defined function called by the LogSnapshot
module whenever it writes an event, the following configuration script
is needed:
var LoggingSetup = xdc.useModule('ti.uia.sysbios.LoggingSetup');
var LogSnapshot = xdc.useModule('ti.uia.runtime.LogSnapshot');
var IUIATraceSyncClient = xdc.useModule('ti.uia.runtime.IUIATraceSyncClient');
LogSnapshot.injectIntoTraceFxn = $externFxn('myHookFxn');
SEE
| config LogSync_maxGlobalClockFreq // module-wide |
 |
The highest bus clock frequency used to drive the timer used for the global
timestamp
DETAILS
The default ticks per second rate of the timer is calculated by dividing
the timer's bus clock frequency by the globalTimestampCpuCyclesPerTick
config parameter.
Defines the highest bus clock frequency used to drive the shared timer used
for the global timestamp.
| LogSync_disable() // module-wide |
 |
Disable logging of sync point events
RETURNS
The function returns the state of the module-level enable (TRUE
if enabled,FALSE if disabled) before the call. This return value
allows clients to restore the previous state.
Note: not thread safe.
| LogSync_enable() // module-wide |
 |
Enables logging of sync point events
RETURNS
The function returns the state of the module-level enable (TRUE
if enabled,FALSE if disabled) before the call. This return value
allows clients to restore the previous state.
Note: not thread safe.
| LogSync_isSyncEventRequired() // module-wide |
 |
Is Sync Event Required
Bool LogSync_isSyncEventRequired();
DETAILS
Checks whether the target has been halted since the
last sync point event and returns true if it has.
RETURN
true if a synchronization event should be logged
| LogSync_putSyncPoint() // module-wide |
 |
Unconditionally put the specified Types event
Void LogSync_putSyncPoint();
DETAILS
This method unconditionally logs a sync point event. It is used
internally by the writeSyncPoint() macro and typically should not be
called directly.
| LogSync_writeSyncPoint() // module-wide |
 |
Log a sync point event along with global timestamp, local CPU frequency
and sync point serial number
macro Void LogSync_writeSyncPoint();
ARGUMENTS
fmt
a constant string that describes why the sync point was
logged.
DETAILS
This method logs a synchronization point event, local CPU timestamp and
global timestamp into the log along with the fmt string a sync point
serial number
| Module-Wide Built-Ins |
 |
// Get this module's unique id
Bool LogSync_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool LogSync_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 LogSync_Module_getMask();
// Returns the diagnostics mask for this module
Void LogSync_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
| Instance Object Types |
 |
typedef struct LogSync_Object LogSync_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct LogSync_Struct LogSync_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
| Instance Config Parameters |
 |
typedef struct LogSync_Params {
// Instance config-params structure
// Common per-instance configs
} LogSync_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
| Instance Built-Ins |
 |
Int LogSync_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object
var LogSync = xdc.useModule('ti.uia.runtime.LogSync');
local proxy modules
module-wide config parameters
per-instance config parameters
| proxy LogSync.CpuTimestampProxy |
 |
CPU Timestamp Proxy
| XDCscript usage |
meta-domain |
// explicit access to the currently bound delegate module
DETAILS
This proxy provides a timestamp server that can be different
from the one provided by
xdc.runtime.Timestamp. However, if
not supplied by a user, this proxy defaults to whichever timestamp
server is provided by
xdc.runtime.Timestamp.
Configuring the CpuTimestampProxy with a local timestamp module
allows applications that change the CPU frequency to report this
information to System Analyzer so that event timestamps can
be adjusted to accommodate the change in frequency.
EXAMPLES
Example: the following configuration script shows how to configure
a C66X Local Timestamp module for use as the CpuTimestampProxy
var TimestampC66Local = xdc.useModule('ti.uia.family.c66.TimestampC66Local');
TimestampC66Local.maxTimerClockFreq = {lo:1200000000,hi:0};
var LogSync = xdc.useModule('ti.uia.runtime.LogSync');
LogSync.CpuTimestampProxy = TimestampC66Local;
| proxy LogSync.GlobalTimestampProxy |
 |
Global Timestamp Proxy
| XDCscript usage |
meta-domain |
// explicit access to the currently bound delegate module
DETAILS
This proxy provides a timestamp server that can be different
from the server provided by
xdc.runtime.Timestamp.
This must be configured in order to use this module.
| config LogSync.cpuTimestampCyclesPerTick // module-wide |
 |
The number of CPU cycles each tick of the global timestamp corresponds to.
0 if no relation between clocks
| XDCscript usage |
meta-domain |
LogSync.cpuTimestampCyclesPerTick = UInt32 1;
DETAILS
If the module configured as the CpuTimestampProxy implements
ti.uia.runtime.IUIATimestampProvider, the default value of this config
option is derived at configuration time from that module's config data.
Otherwise it is initialized to 0 to signify that there is no way to
convert a number of global timestamp tick counts into an equivalent
number of CPU cycles.
C SYNOPSIS
| config LogSync.globalTimestampCpuCyclesPerTick // module-wide |
 |
The number of CPU cycles each tick of the global timestamp corresponds
to. 0 if no relation between clocks
| XDCscript usage |
meta-domain |
LogSync.globalTimestampCpuCyclesPerTick = UInt32 0;
DETAILS
A value of 0 signifies that there is no way to convert a number of
global timestamp tick counts into an equivalent number of CPU cycles.
Note that this value will be automatically copied from the
GlobalTimestampProxy.cpuCyclesPerTick configuration value
at configuration time if GlobalTimestampProxy.cpuCyclesPerTick > 0.
C SYNOPSIS
| config LogSync.injectIntoTraceFxn // module-wide |
 |
Callback function that handles injection of info such as serial numbers
of sync point events, context change events or snapshot events into a
hardware trace stream. (e.g. GEM CPU Trace, System Trace, etc.)
| XDCscript usage |
meta-domain |
DETAILS
Users can provide their own custom injectIntoTraceFxn to log whatever
additional information they wish to record when the hook function is called.
For example, event serial numbers can be injected into the CPU
trace stream and / or STM trace stream in order to enable correlation
of information logged in these streams with UIA software events.
EXAMPLES
Example 1: Correlating events with C64X+ and C66 CPU Trace
The following is an example of the configuration script used
to inject serial numbers of sync point events or context change events or
snapshot Ids associated with snapshot events.
Note that the GemTraceSync module's .xs script takes care of finding
all modules that implement the IUIATraceSyncClient and assigning the
GemTraceSync_injectIntoTrace function pointer to those modules'
injectIntoTraceFxn config option.
//The following 3 modules all implement the IUIATraceSyncClient interface
var LogSnapshot = xdc.useModule('ti.uia.runtime.LogSnapshot');
var LogCtxChg = xdc.useModule('ti.uia.runtime.LogCtxChg');
var LogSync = xdc.useModule('ti.uia.runtime.LogSync');
//For C66 devices, replace the following line with
// var GemTraceSync = xdc.useModule('ti.uia.family.c66.GemTraceSync');
var GemTraceSync = xdc.useModule('ti.uia.family.c64p.GemTraceSync');
Example 2: How to create a custom hook function
and assign it to the LogSnapshot module
The following is an example of a 'C' code program that implements
a hook function that prints out the snapshot ID that is passed in
as the serialNumber
#include <xdc/std.h>
#include <xdc/runtime/Gate.h>
#include <ti/uia/runtime/IUIATraceSyncProvider.h>
#include <ti/uia/runtime/LogSnapshot.h>
#include <stdio.h>
#include <string.h>
extern Void myHookFxn(UInt32 serialNumber, IUIATraceSyncProvider_ContextType ctxType);
Void Test();
char name[32]={"Bob"};
UInt32 newAppId = 0;
Void myHookFxn(UInt32 serialNumber, IUIATraceSyncProvider_ContextType ctxType){
volatile UInt32 syncWord;
IArg key = Gate_enterSystem();
printf("newAppId written with serialNumber %d and ctxType = %d\n",serialNumber,ctxType);
Gate_leaveSystem(key);
}
Void Test(){
// note that the hook function is triggered by calling LogSnapshot_getSnapshotId()
// since that is where the unique snapshot ID that is passed to the
// hook function is generated.
Int snapshotId = LogSnapshot_getSnapshotId();
LogSnapshot_writeString(snapshotId,"User-defined name=%s.",name, strlen(name));
}
Void main(){
while(TRUE){ Test(); }
}
In order to have the above user-defined function called by the LogSnapshot
module whenever it writes an event, the following configuration script
is needed:
var LoggingSetup = xdc.useModule('ti.uia.sysbios.LoggingSetup');
var LogSnapshot = xdc.useModule('ti.uia.runtime.LogSnapshot');
var IUIATraceSyncClient = xdc.useModule('ti.uia.runtime.IUIATraceSyncClient');
LogSnapshot.injectIntoTraceFxn = $externFxn('myHookFxn');
SEE
C SYNOPSIS
| config LogSync.maxGlobalClockFreq // module-wide |
 |
The highest bus clock frequency used to drive the timer used for the global
timestamp
| XDCscript usage |
meta-domain |
DETAILS
The default ticks per second rate of the timer is calculated by dividing
the timer's bus clock frequency by the globalTimestampCpuCyclesPerTick
config parameter.
Defines the highest bus clock frequency used to drive the shared timer used
for the global timestamp.
C SYNOPSIS
| metaonly config LogSync.canCpuCyclesPerTickBeChanged // module-wide |
 |
Indicates whether the CPU timer's cycles per tick divide down ratio can
be changed or not
| XDCscript usage |
meta-domain |
LogSync.canCpuCyclesPerTickBeChanged = Bool false;
DETAILS
Set to true if the timer's CPU cycles per tick can be changed
| metaonly config LogSync.canCpuFrequencyBeChanged // module-wide |
 |
Indicates whether the timer frequency can be changed or not
| XDCscript usage |
meta-domain |
LogSync.canCpuFrequencyBeChanged = Bool false;
DETAILS
Set to true if the timer's clock frequency can be changed
| metaonly config LogSync.common$ // module-wide |
 |
Common module configuration parameters
| XDCscript usage |
meta-domain |
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
| metaonly config LogSync.defaultSyncLoggerSize // module-wide |
 |
Configures the size of the default syncLogger created by LogSync
| XDCscript usage |
meta-domain |
LogSync.defaultSyncLoggerSize = SizeT 256;
DETAILS
Only used if syncLogger is null.
| metaonly config LogSync.enableEventCorrelationForJTAG // module-wide |
 |
Enable event correlation for JTAG Transports
| XDCscript usage |
meta-domain |
LogSync.enableEventCorrelationForJTAG = Bool false;
DETAILS
By default, event correlation is disabled for JTAG transports.
In order for event correlation to work with JTAG transports,
it is necessary for the target program to periodically execute
the following code (e.g. from a low priority thread) in order
to log enough synchronization information to reestablish event
correlation after a breakpoint has been hit.
C code:
#include <xdc/std.h>
#include <ti/uia/runtime/LogSync.h>
...
if (LogSync_isSyncEventRequired()){
LogSync_writeSyncPoint();
}
Since most JTAG debugging sessions start with a breakpoint being
hit at main, event correlation will only be possible once a sync
point event has been logged after running from main. Calling the
above code snippet as part of the code that is run by main is
highly recommended in order to establish synchronization information
as early in the program's execution as possible.
| metaonly config LogSync.isEnabled // module-wide |
 |
Configures whether sync logging is enabled (true) or disabled (false)
| XDCscript usage |
meta-domain |
LogSync.isEnabled = Bool true;
| metaonly config LogSync.isInjectIntoTraceEnabled // module-wide |
 |
set false to turn off injection of sync point info into trace even
if a module that implements IUIATraceSyncProvider is configured
| XDCscript usage |
meta-domain |
LogSync.isInjectIntoTraceEnabled = Bool true;
DETAILS
The XDCScript associated with a module that implements IUIATraceSyncProvider
is responsible for checking this config option for all IUIATraceSyncClient
modules before automatically configuring the client callback function.
This allows users to control which features have sync points injected
into the trace stream. For example, a user may wish to configure
LogSync.isInjectIntoTraceEnabled = true and
LogCtxChg.isInjectIntoTraceEnabled = false in order to reduce the number
of sync point events injected into the trace stream.
| metaonly config LogSync.maxCpuClockFreq // module-wide |
 |
The highest bus clock frequency used to drive the timer
| XDCscript usage |
meta-domain |
DETAILS
The default ticks per second rate of the timer is calculated by dividing
the timer's bus clock frequency by the cpuTimestampCyclesPerTick
config parameter.
Defines the 32 MSBs of the highest bus clock frequency used to drive
the timer.
| metaonly config LogSync.syncLogger // module-wide |
 |
Configures the logger instance to use to log sync point events
| XDCscript usage |
meta-domain |
DETAILS
If left null, an instance of LoggerStopMode will be created for
dedicated use by the LogSync module in order to log sync point events.
(The ti.uia.services.Rta and ti.uia.sysbios.LoggerSetup modules
can specify that the LoggerCircBuf module be used as the default
if the user has specified a non-JTAG transport for event upload.)
| Instance Config Parameters |
 |
| XDCscript usage |
meta-domain |
var params = new LogSync.Params;
// Instance config-params object
generated on Wed, 26 Oct 2011 00:41:34 GMT