A loggerSnapshot is responsible for recording, transmitting, or otherwise
handling
LogSnapshot Events generated by clients of the
LogSnapshot module. The
LogSnapshot module uses modules that implement the
ILoggerSnapshot interface to record the log events. Most application code will
use the
LogSnapshot module instead of directly calling the specific
ILoggerSnapshot
module implementation.
All loggerSnapshot implementations must inherit from this interface. The
derived implementations must implement the functions defined in this
interface but may also add additional configuration parameters and
functions.
| enum ILoggerSnapshot.TransferType |
 |
enum TransferType {
TransferType_RELIABLE,
TransferType_LOSSY
};
| metaonly struct ILoggerSnapshot.MetaData |
 |
This data is added to the RTA MetaData file to support stop mode RTA
metaonly struct MetaData {
Int instanceId;
Int priority;
};
| config ILoggerSnapshot.filterByLevel // module-wide |
 |
Support filtering of events by event level
config Bool filterByLevel = false;
DETAILS
To improve logging performance, this feature can be disabled by setting
filterByLevel to false.
See '
setFilterLevel' for an explanation of level filtering.
| metaonly config ILoggerSnapshot.common$ // module-wide |
 |
Common module configuration parameters
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
| metaonly ILoggerSnapshot.getLoggerInstanceId() // module-wide |
 |
returns the id of this logger instance
metaonly function getLoggerInstanceId(inst);
| metaonly ILoggerSnapshot.getMetaArgs() // module-wide |
 |
Returns any meta data needed to support RTA
metaonly function getMetaArgs(inst, instNum);
DETAILS
This meta data should be returned in the form of a structure which
can be converted into XML. This data is added to the RTA XML file
during the application's configuration, and can be accessed later
through the xdc.rta.MetaData module.
The MetaData is returned per instance of the ILogger module. The
instance object is passed to the function as the first argument.
The second argument is the index of the instance in the list of
the ILogger's static instances.
| metaonly ILoggerSnapshot.getPtrToQueueDescriptorMeta() // module-wide |
 |
Each logger instance has a unique queue descriptor address that is
stored in the Event Record header to identify itself to the host.
This metaonly configuration parameter allows the UIA Metadata to
determine what the address is for each statically created logger instance
in order to emit XML code to allow the host to look up information about
the logger instance (such as its name) based on the queue descriptor
address that is stored in the event record header
metaonly function getPtrToQueueDescriptorMeta(inst);
DETAILS
The pointer is returned per instance of the logger module. The
instance object is passed to the function as the first argument.
| metaonly ILoggerSnapshot.setPtrToQueueDescriptorMeta() // module-wide |
 |
Sets the queue descriptor address in the logger's object instance data
metaonly function setPtrToQueueDescriptorMeta(inst, queueDescriptorAdrs);
| config ILoggerSnapshot.transferType // instance |
 |
| metaonly config ILoggerSnapshot.ptrToQueueDescriptorMeta // instance |
 |
metaonly config Ptr ptrToQueueDescriptorMeta = null;
| ILoggerSnapshot.disable() // instance |
 |
Disable a log
DETAILS
Events written to a disabled log are silently discarded.
RETURNS
The function returns the state of the log (TRUE if enabled,
FALSE if disabled) before the call. This return value allows
clients to restore the previous state.
Note: not thread safe.
| ILoggerSnapshot.enable() // instance |
 |
Enable a log
RETURNS
The function returns the state of the log (TRUE if enabled,
FALSE if disabled) before the call. This return value allows
clients to restore the previous state.
Note: not thread safe.
| ILoggerSnapshot.getContents() // instance |
 |
Fills buffer that is passed in with unread data, up to size bytes
in length
Bool getContents(Ptr hdrBuf, SizeT size, SizeT *cpSize);
ARGUMENTS
hdrBuf
Ptr to a buffer that is at least <size> bytes in length
size
The max number of bytes to be read into the buffer
cpSize
The number of bytes actually copied
DETAILS
The logger is responsible for ensuring that no partial event records
are stored in the buffer. Bytes are in target endianness.
RETURN
returns false if logger has no more records to read
| ILoggerSnapshot.getFilterLevel() // instance |
 |
Returns the mask of diags categories currently set to the specified
level
DETAILS
See '
setFilterLevel' for an explanation of level filtering.
| ILoggerSnapshot.getInstanceId() // instance |
 |
Returns an ID value that uniquely identifies this instance of the logger
DETAILS
Note that a value of 0 is reserved to indicate that the instance ID has
not been initialized yet and a unique value needs to be generated.
| ILoggerSnapshot.getMaxLength() // instance |
 |
| ILoggerSnapshot.getTransferType() // instance |
 |
| ILoggerSnapshot.isEmpty() // instance |
 |
Returns true if the transfer buffer has no unread data
RETURN
true if no unread data
| ILoggerSnapshot.reset() // instance |
 |
Reset a log to empty state and enable it
WARNING
This method is not synchronized with other instance
methods and, as a result, it must never be called when there is a
chance that another instance method is currently in operation or
when another method on this instance may preempt this call.
| ILoggerSnapshot.setFilterLevel() // instance |
 |
Set the level of detail that instances will log
ARGUMENTS
mask
The diags categories to set the level for
filterLevel
The new filtering level for the specified
categories
DETAILS
Events with the specified level or higher will be logged, events
below the specified level will be dropped.
Events are filtered first by diags category, then by level. If an
event's diags category is disabled in the module's diags mask, then it
will be filtered out regardless of level. The event will not even be
passed to the logger.
This API allows for setting the filtering level for more than one
diags category at a time. The mask parameter can be a single category
or multiple categories combined, and the level will be set for all of
those categories.
| ILoggerSnapshot.write0() // instance |
 |
Process a log event with 0 arguments
DETAILS
Same as write4 except with 0 arguments rather than 4.
SEE
| ILoggerSnapshot.write1() // instance |
 |
Process a log event with 1 arguments
DETAILS
Same as write4 except with 1 arguments rather than 4.
SEE
| ILoggerSnapshot.write2() // instance |
 |
Process a log event with 2 arguments
DETAILS
Same as write4 except with 2 arguments rather than 4.
SEE
| ILoggerSnapshot.write4() // instance |
 |
Process a log event with up to 4 arguments
ARGUMENTS
evt
event to be logged
mid
module ID of the module which logged the event
a1
arbitrary argument passed by caller
DETAILS
The
evt argument is of type Log.Event, which encodes the
Log.EventId, the
Diags.Mask, and the
Diags.EventLevel of the event. The event ID can be obtained
via
Types.getEventId(evt), the Diags mask can be obtained via
Diags.getMask(evt), and the event level can be obtained via
Diags.getLevel(evt).
The modId argument is the module ID of the module that logged the
event.
The event information can be used by the logger to handle different
events specially. For example, the event ID can be used to compare
against other known Log.Events.
if (Log_getEventId(MY_EVENT) == Log_getEventId(evt)) {
:
}
The Diags mask and event level can be used for filtering of events
based on event level (see
IFilterLogger), or even routing
events to separate loggers based on diags category (see, for example,
LoggerBuf.statusLogger).
The Diags mask and event level are useful for handling the event, but
are generally not recorded by the logger because they are not needed in
decoding and displaying the event. A more suitable value to record is a
Types.Event, which encodes the event ID and module ID. For
example, the
Log.EventRec type stores a
Types.Event
in its record definition. A
Types.Event can be created using
the
Types.makeEvent API given the event ID and module ID.
The event ID value of
0 is used to indicate an event triggered by a
call to one of the
Log_print[0-6] methods. These
methods take a format string rather than a
Log_Event argument and,
as a result, the event ID encoded in
evt is
0 and the parameter
a1 is the format string.
Non-zero event IDs can also be used to access the
msg string
associated with the
Log.EventDesc that originally
defined the
Log event.
Log_EventId id = Log_getEventId(evt));
if (id != 0) {
String msg = Text_ropeText(id);
System_aprintf(msg, a1, a2, a3, a4);
}
This works because an event's ID is simply an offset into a table
of characters (maintained by the
Text module)
containing the event's msg string.
The arguments a1, a2, etc. are parameters that are to be interpreted
according to the message format string associated with evt.
SEE
| ILoggerSnapshot.write8() // instance |
 |
Process a log event with up to 8 arguments
Void write8(
Log.Event evt,
Types.ModuleId mid,
IArg a1,
IArg a2,
IArg a3,
IArg a4,
IArg a5,
IArg a6,
IArg a7,
IArg a8);
DETAILS
Same as write4 except with 8 arguments rather than 4.
SEE
| ILoggerSnapshot.writeMemoryRange() // instance |
 |
Log an event along with values from a range of memory addresses
Void writeMemoryRange(
Log.Event evt,
Types.ModuleId mid,
UInt32 snapshotId,
IArg fileName,
IArg LineNum,
IArg fmt,
IArg startAdrs,
UInt32 lengthInMAUs);
ARGUMENTS
evt
event to be logged
snapshotId
0 = no other snapshot groups, Use value from
LogSnapshot.getSnapshotId() for all snapshots to be grouped.
fileName
__FILE__ result
lineNum
__LINE__ result
fmt
a printf style format string
startAdrs
value for first format conversion character
lengthInMAUs
value for second format conversion character
DETAILS
If the mask in the specified LogSnapshot event has any bit set which is
also set in the current module's diagnostics mask, then this call to
write will "raise" the given LogSnapshot event.
Note that this API supports null terminated strings, arrays of characters and
memory mapped registgers as well as blocks of memory. The LogSnapshot module provides macros that
map the appropriate values to the writeMemoryRange API's arguments
SEE