| module ti.uia.events.UIAThreadCtx |
 |
 |
 |
UIA Thread Context Instrumentation
The UIAThreadCtx module defines context change events
and methods that allow tooling to identify thread context
switches and to enable thread-aware filtering, trace and
analysis.
[
more ... ]
#include <ti/uia/events/UIAThreadCtx.h>
Functions |
macro Int | |
Bool | |
UInt | |
Functions common to all target modules |
|
|
Typedefs |
typedef Bool | |
Constants |
| |
| |
extern const Bits16 | |
| |
extern const Bits16 | |
DETAILS
The UIAThreadCtx module defines context change events
and methods that allow tooling to identify thread context
switches and to enable thread-aware filtering, trace and
analysis.
It inherits IUIACtx, which defines a function pointer to
an isLoggingEnabled function which, if configured to point to
a function, will evaluate the function prior to logging the context
change event and will store the return value of the function in
ti_uia_runtime_CtxFilter_gIsLoggingEnabled, which is used to
determine whether or not to log events.
The generation of UIAThreadCtx events is also controlled by a module's diagnostics
mask, which is described in details in
xdc.runtime.Diags.
'UIAThreadCtx` events are generated only when the Diags.ANALYSIS bit is set
in the module's diagnostics mask.
The following configuration script demonstrates how the application might
control the logging of ANALYSIS events embedded in the Mod module at configuration
time. In this case, the configuration script arranges for the Log
statements within modules to always generate ANALYSIS events.
Without these configuration statements, no ANALYSIS events would be generated
by any modules.
EXAMPLES
Example 1: This is part of the XDC configuration file for the application:
var LogCtxChg = xdc.useModule('ti.uia.runtime.LogCtxChg');
var Diags = xdc.useModule('xdc.runtime.Diags');
var LoggerSys = xdc.useModule('xdc.runtime.LoggerSys');
var Defaults = xdc.useModule('xdc.runtime.Defaults');
var logger = LoggerSys.create();
Defaults.common$.diags_ANALYSIS = Diags.ALWAYS_ON;
Defaults.common$.logger = logger;
Example 2: The following example configures a module to support logging
of ANALYSIS events, but defers the actual activation and deactivation of the
logging until runtime. See the
Diags_setMask()
function for details on specifying the control string.
This is a part of the XDC configuration file for the application:
var LogCtxChg = xdc.useModule('ti.uia.runtime.LogCtxChg');
var Diags = xdc.useModule('xdc.runtime.Diags');
var Mod = xdc.useModule('my.pkg.Mod');
Mod.common$.diags_ANALYSIS = Diags.RUNTIME_OFF;
This is a part of the C code for the application:
// turn on logging of ANALYSIS events in the module
Diags_setMask("my.pkg.Mod+Z");
// turn off logging of ANALYSIS events in the module
Diags_setMask("my.pkg.Mod-Z");
| typedef UIAThreadCtx_IsLoggingEnabledFxn |
 |
typedef Bool (*UIAThreadCtx_IsLoggingEnabledFxn)(Int);
| config UIAThreadCtx_ENABLEMASK // module-wide |
 |
Ctx Filter Enable Mask
extern const Bits16 UIAThreadCtx_ENABLEMASK;
DETAILS
configures which bit of the ti_uia_runtime_CtxFilter_gFlags
is assigned to control context aware filtering for
frame context changes. Must be configured with a
value that is 2**SYNCID.
| config UIAThreadCtx_SYNCID // module-wide |
 |
Trace Synchronization ID
extern const Bits16 UIAThreadCtx_SYNCID;
DETAILS
configures the value to be written into the
4 bit context change type field used by the
UIASync trace synchronization
| config UIAThreadCtx_ctxChg // module-wide |
 |
threadSwitch Context Change event
VALUES
fmt
a constant string that describes the context change and provides a format specifier for newThreadId
newThreadId
an integer which uniquely identifies the new context
DETAILS
Used to log a thread switch
Note that the previous thread Id is logged automatically by the ti_uia_runtime_LogCtxChg_thread
API.
If ti_uia_events_UIAThreadCtx_isLoggingEnabledFxn is not NULL
it is called and its return value determines whether logging is enabled or not.
EXAMPLE
The following C code shows how to log a Thread Context Change
event that identifies a new thread using a BIOS task switch hook function
#include <ti/uia/runtime/LogCtxChg.h>
...
Void tskSwitchHook(Task_Handle hOldTask,Task_Handle hNewTask){
LogCtxChg_thread("thread: new = 0x%x",(Int)hNewTask);
}
This event prints the Log call site (%$F) and a format string (%$S)
which is recursively formatted with any addition arguments.
The following text is an example of what will be displayed for the event:
"Thread Ctx Change at Line 123 in demo.c [Prev. thread ID=0x1234] New thread ID=0x1235"
| config UIAThreadCtx_ctxChgWithFunc // module-wide |
 |
threadSwitch Context Change event with prempted function and resumed function addresses
extern const Log_Event UIAThreadCtx_ctxChgWithFunc;
VALUES
fmt
a constant string that describes the context change and provides a format specifier for newThreadId
newThreadId
an integer which uniquely identifies the new context
oldFunc
the address of the function that was preempted
newFunc
the address of the function that is being resumed
DETAILS
Used to log a thread switch along with function info (preempted function and new function)
Note that the previous thread Id is logged automatically by the ti_uia_runtime_LogCtxChg_threadAndFunc
API.
If ti_uia_events_UIAThreadCtx_isLoggingEnabledFxn is not NULL
it is called and its return value determines whether logging is enabled or not.
EXAMPLE
The following C code shows how to log a Thread Context Change
event that identifies a new thread, the preempted function and the preempting function.
#include <ti/uia/runtime/LogCtxChg.h>
...
LogCtxChg_threadAndFunc("New thread ID=0x%x, oldFunc=0x%x, newFunc=0x%x",(Int)hNewTask, (Int)&oldFunc,(Int)&newFunc);
This event prints the Log call site (%$F) and a format string (%$S)
which is recursively formatted with any addition arguments.
The following text is an example of what will be displayed for the event:
"Thread CtxChgWithFunc at Line 123 in demo.c [Prev. thread ID=0x1234] New thread ID=0x1235, oldFunc=0x80001200, newFunc=0x80001080"
| config UIAThreadCtx_isLoggingEnabledFxn // module-wide |
 |
| UIAThreadCtx_getCtxId() // module-wide |
 |
Get the ID for the current thread
macro Int UIAThreadCtx_getCtxId();
RETURNS
returns the thread ID logged by the last call to UIAThreadCtx_logCtxChg.
| UIAThreadCtx_isLoggingEnabled() // module-wide |
 |
returns true if the new context matches the value to enable logging with
Bool UIAThreadCtx_isLoggingEnabled(UInt newThreadId);
ARGUMENTS
newThreadId
the new thread ID
DETAILS
Default implementation of the IUIACtx_IsLoggingEnabledFxn for user context.
To enable context-aware filtering, assign UIAThreadCtx_isLoggingEnabledFxn = &UIAThreadCtx_isLoggingEnabled
in the config script or programmatically, or assign your own implementation of this
function.
RETURNS
true if logging is enabled
| UIAThreadCtx_setOldValue() // module-wide |
 |
sets ti_uia_events_UIAThreadCtx_gLastValue to the new value and returns the old value before it was updated
UInt UIAThreadCtx_setOldValue(UInt newValue);
ARGUMENTS
newValue
the new value to save in the global variable
(return0 the original value of the global variable before it was updated.
| Module-Wide Built-Ins |
 |
// Get this module's unique id
Bool UIAThreadCtx_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool UIAThreadCtx_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 UIAThreadCtx_Module_getMask();
// Returns the diagnostics mask for this module
Void UIAThreadCtx_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
var UIAThreadCtx = xdc.useModule('ti.uia.events.UIAThreadCtx');
module-wide config parameters
msg: "Thread Ctx Change at %$F [Prev. thread ID = 0x%x] %$S"
};
msg: "Thread CtxChgWithFunc at %$F [Prev. threadId = 0x%x] %$S"
};
| config UIAThreadCtx.ENABLEMASK // module-wide |
 |
Ctx Filter Enable Mask
| XDCscript usage |
meta-domain |
UIAThreadCtx.ENABLEMASK = Bits16 undefined;
DETAILS
configures which bit of the ti_uia_runtime_CtxFilter_gFlags
is assigned to control context aware filtering for
frame context changes. Must be configured with a
value that is 2**SYNCID.
C SYNOPSIS
| config UIAThreadCtx.SYNCID // module-wide |
 |
Trace Synchronization ID
| XDCscript usage |
meta-domain |
UIAThreadCtx.SYNCID = Bits16 undefined;
DETAILS
configures the value to be written into the
4 bit context change type field used by the
UIASync trace synchronization
C SYNOPSIS
| config UIAThreadCtx.ctxChg // module-wide |
 |
threadSwitch Context Change event
| XDCscript usage |
meta-domain |
msg: "Thread Ctx Change at %$F [Prev. thread ID = 0x%x] %$S"
};
VALUES
fmt
a constant string that describes the context change and provides a format specifier for newThreadId
newThreadId
an integer which uniquely identifies the new context
DETAILS
Used to log a thread switch
Note that the previous thread Id is logged automatically by the ti_uia_runtime_LogCtxChg_thread
API.
If ti_uia_events_UIAThreadCtx_isLoggingEnabledFxn is not NULL
it is called and its return value determines whether logging is enabled or not.
EXAMPLE
The following C code shows how to log a Thread Context Change
event that identifies a new thread using a BIOS task switch hook function
#include <ti/uia/runtime/LogCtxChg.h>
...
Void tskSwitchHook(Task_Handle hOldTask,Task_Handle hNewTask){
LogCtxChg_thread("thread: new = 0x%x",(Int)hNewTask);
}
This event prints the Log call site (%$F) and a format string (%$S)
which is recursively formatted with any addition arguments.
The following text is an example of what will be displayed for the event:
"Thread Ctx Change at Line 123 in demo.c [Prev. thread ID=0x1234] New thread ID=0x1235"
C SYNOPSIS
| config UIAThreadCtx.ctxChgWithFunc // module-wide |
 |
threadSwitch Context Change event with prempted function and resumed function addresses
| XDCscript usage |
meta-domain |
msg: "Thread CtxChgWithFunc at %$F [Prev. threadId = 0x%x] %$S"
};
VALUES
fmt
a constant string that describes the context change and provides a format specifier for newThreadId
newThreadId
an integer which uniquely identifies the new context
oldFunc
the address of the function that was preempted
newFunc
the address of the function that is being resumed
DETAILS
Used to log a thread switch along with function info (preempted function and new function)
Note that the previous thread Id is logged automatically by the ti_uia_runtime_LogCtxChg_threadAndFunc
API.
If ti_uia_events_UIAThreadCtx_isLoggingEnabledFxn is not NULL
it is called and its return value determines whether logging is enabled or not.
EXAMPLE
The following C code shows how to log a Thread Context Change
event that identifies a new thread, the preempted function and the preempting function.
#include <ti/uia/runtime/LogCtxChg.h>
...
LogCtxChg_threadAndFunc("New thread ID=0x%x, oldFunc=0x%x, newFunc=0x%x",(Int)hNewTask, (Int)&oldFunc,(Int)&newFunc);
This event prints the Log call site (%$F) and a format string (%$S)
which is recursively formatted with any addition arguments.
The following text is an example of what will be displayed for the event:
"Thread CtxChgWithFunc at Line 123 in demo.c [Prev. thread ID=0x1234] New thread ID=0x1235, oldFunc=0x80001200, newFunc=0x80001080"
C SYNOPSIS
| config UIAThreadCtx.isLoggingEnabledFxn // module-wide |
 |
| XDCscript usage |
meta-domain |
UIAThreadCtx.isLoggingEnabledFxn = Bool(*)(Int) null;
C SYNOPSIS
| metaonly config UIAThreadCtx.common$ // module-wide |
 |
Common module configuration parameters
| XDCscript usage |
meta-domain |
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
generated on Wed, 26 Oct 2011 00:41:23 GMT