| module ti.uia.events.UIAStatistic |
 |
 |
 |
UIA Statistics Events
The UIAStatistic module defines events that allow
tooling to analyze the performance of the software
(CPU Utilization, throughput, etc.)
[
more ... ]
#include <ti/uia/events/UIAStatistic.h>
Functions common to all target modules |
|
|
Constants |
| |
| |
| |
| |
| |
| |
| |
DETAILS
The UIAStatistic module defines events that allow
tooling to analyze the performance of the software
(CPU Utilization, throughput, etc.)
The generation of UIAStatistic events is controlled by a module's diagnostics
mask, which is described in details in
xdc.runtime.Diags.
UIAStatistic events are generated only when the Diags.ANALYSIS bit is set
in the module's diagnostics mask.
The following configuration script demonstrates how the application might
control the logging of ANALYSIS events embedded in the Mod module at configuration
time. In this case, the configuration script arranges for the Log
statements within modules to always generate ANALYSIS events.
Without these configuration statements, no ANALYSIS events would be generated
by any modules.
EXAMPLES
Example 1: This is part of the XDC configuration file for the application:
var UIAStatistic = xdc.useModule('ti.uia.events.UIAStatistic');
var Diags = xdc.useModule('xdc.runtime.Diags');
var LoggerSys = xdc.useModule('xdc.runtime.LoggerSys');
var Defaults = xdc.useModule('xdc.runtime.Defaults');
var logger = LoggerSys.create();
Defaults.common$.diags_ANALYSIS = Diags.ALWAYS_ON;
Defaults.common$.logger = logger;
Example 2: The following example configures a module to support logging
of ANALYSIS events, but defers the actual activation and deactivation of the
logging until runtime. See the
Diags_setMask()
function for details on specifying the control string.
This is a part of the XDC configuration file for the application:
var UIAStatistic = xdc.useModule('ti.uia.events.UIAStatistic');
var Diags = xdc.useModule('xdc.runtime.Diags');
var Mod = xdc.useModule('my.pkg.Mod');
Mod.common$.diags_ANALYSIS = Diags.RUNTIME_OFF;
This is a part of the C code for the application:
// turn on logging of ANALYSIS events in the module
Diags_setMask("my.pkg.Mod+Z");
// turn off logging of ANALYSIS events in the module
Diags_setMask("my.pkg.Mod-Z");
| config UIAStatistic_bytesProcessed // module-wide |
 |
bytesProcessed statistic event
extern const Log_Event UIAStatistic_bytesProcessed;
VALUES
name
a constant string that provides the name
of the entity that is processing the data
numBytes
the number of bytes processed
DETAILS
Number of bytes that were processed.
| config UIAStatistic_bytesProcessedByInstance // module-wide |
 |
bytesProcessedByInstance statistic event
extern const Log_Event UIAStatistic_bytesProcessedByInstance;
VALUES
__FILE__
constant string identifying the file the event was logged from
__LINE__
the line number the event was logged from
instanceId
the instance ID (e.g. thread handle) of the
entity that is processing the data
numBytes
the number of bytes processed
DETAILS
Number of bytes that were processed along with filename,
line number and instance ID.
EXAMPLE
The following C code shows how to log an
event that tracks the number of bytes processed
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAStatistic.h>
...
Void myFunction(){
int instanceId = 0x1234; // change to e.g. a TaskId or some other unique ID
int numBytes= 567; // change to number of bytes actually processed
Log_write4(UIAStatistic_bytesProcessedByInstance, (IArg)__FILE__,(IArg)__LINE__,instanceId,numBytes);
}
The following text will be displayed for the event:
Bytes Processed at Line 123 in demo.c (InstanceId 0x1234): Num Bytes=567
| config UIAStatistic_cpuLoad // module-wide |
 |
Number of cycles used by an XDC module
VALUES
numCycles
the CPU load in cycles
EXAMPLE
The following C code shows how to log a cpuLoad
event that tracks the number of cycles used by an XDC module.
The module ID is logged along with the event. For non-XDC
code, or for code with multiple instances @see #cpuLoadByInstance.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAStatistic.h>
...
Void myFunction(){
int numCycles = 0;
// update numCycles with the number of cycles processed
Log_write1(UIAStatistic_cpuLoad, numCycles);
}
The following text will be displayed for the event:
| config UIAStatistic_cpuLoadByInstance // module-wide |
 |
Number of cycles used by a non XDC module or thread
extern const Log_Event UIAStatistic_cpuLoadByInstance;
VALUES
name
a constant string that provides the name of the entity that is processing the data
instanceId
the instance ID (e.g. thread handle) of the entity that is processing the data
numCycles
the CPU load in cycles
EXAMPLE
The following C code shows how to log a cpuLoad
event that tracks the number of cycles used by
code that is not in an XDC module or by a thread
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAStatistic.h>
static volatile int gMyGlobalInstanceId = 0;
...
Void myFunction(){
IArg key;
int localInstanceId;
int numCycles = 0;
// protect pre-increment operation from race conditions
key = Gate_enterSystem();
localInstanceId = ++gMyGlobalInstanceId;
Gate_leaveSystem(key);
// update numCycles with the number of cycles processed
Log_write3(UIAStatistic_cpuLoadByInstance, "myFunction",localInstanceId,numCycles);
}
The following text will be displayed for the event:
CPU Load for myFunction (instanceId = 0x1234): NumCycles=1234
| config UIAStatistic_freeBytes // module-wide |
 |
Number of free bytes in heap
extern const Log_Event UIAStatistic_freeBytes;
VALUES
__FILE__
constant string identifying the file the event was logged from
__LINE__
the line number the event was logged from
heapId
heap identifier (e.g IHeap_Handle)
freeBytes
the number of bytes free on the heap
EXAMPLE
The following C code shows how to log a freeBytes
event that tracks the number of bytes free in the heap
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAStatistic.h>
...
Void myFunction(){
int heapId = 0x1234; // change to heap ID
int numBytesFree = 567; // change to number of bytes free on the heap
Log_write4(UIAStatistic_freeBytes, (IArg)__FILE__,(IArg)__LINE__,heapId,numFreeBytes);
}
The following text will be displayed for the event:
Heap at Line 123 in demo.c (HeapId 0x1234): Free Bytes=567
| config UIAStatistic_wordsProcessed // module-wide |
 |
wordsProcessed statistic event
extern const Log_Event UIAStatistic_wordsProcessed;
VALUES
name
a constant string that provides the name
of the entity that is processing the data
numWords
the number of words processed
DETAILS
number of words that were processed.
| config UIAStatistic_wordsProcessedByInstance // module-wide |
 |
wordsProcessedByInstance statistic event
extern const Log_Event UIAStatistic_wordsProcessedByInstance;
VALUES
__FILE__
constant string identifying the file the event was logged from
__LINE__
the line number the event was logged from
instanceId
the instance ID (e.g. thread handle) of the
entity that is processing the data
numWords
the number of words processed
DETAILS
Number of words that were processed along with filename,
line number and instance ID.
EXAMPLE
The following C code shows how to log an
event that tracks the number of words processed
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAStatistic.h>
...
Void myFunction(){
int instanceId = 0x1234; // change to e.g. a TaskId or some other unique ID
int numWords= 567; // change to number of words actually processed
Log_write4(UIAStatistic_wordsProcessedByInstance, (IArg)__FILE__,(IArg)__LINE__,instanceId,numWords);
}
The following text will be displayed for the event:
Words Processed at Line 123 in demo.c (InstanceId 0x1234): Num Words=567
| Module-Wide Built-Ins |
 |
// Get this module's unique id
Bool UIAStatistic_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool UIAStatistic_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 UIAStatistic_Module_getMask();
// Returns the diagnostics mask for this module
Void UIAStatistic_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
var UIAStatistic = xdc.useModule('ti.uia.events.UIAStatistic');
module-wide config parameters
msg: "Bytes Processed by %s: NumBytes=0x%x"
};
msg: "Bytes Processed at %$F (InstanceId 0x%x): Num Bytes=%d"
};
msg: "CPU Load: NumCycles=%d"
};
msg: "CPU Load for %s (instanceId = 0x%x): NumCycles=%d"
};
msg: "Heap at %$F (HeapId 0x%x): Free Bytes=%d"
};
msg: "Words Processed by %s: NumWords=0x%x"
};
msg: "Words Processed at %$F (InstanceId 0x%x): Num Words=%d"
};
| config UIAStatistic.bytesProcessed // module-wide |
 |
bytesProcessed statistic event
| XDCscript usage |
meta-domain |
msg: "Bytes Processed by %s: NumBytes=0x%x"
};
VALUES
name
a constant string that provides the name
of the entity that is processing the data
numBytes
the number of bytes processed
DETAILS
Number of bytes that were processed.
C SYNOPSIS
| config UIAStatistic.bytesProcessedByInstance // module-wide |
 |
bytesProcessedByInstance statistic event
| XDCscript usage |
meta-domain |
msg: "Bytes Processed at %$F (InstanceId 0x%x): Num Bytes=%d"
};
VALUES
__FILE__
constant string identifying the file the event was logged from
__LINE__
the line number the event was logged from
instanceId
the instance ID (e.g. thread handle) of the
entity that is processing the data
numBytes
the number of bytes processed
DETAILS
Number of bytes that were processed along with filename,
line number and instance ID.
EXAMPLE
The following C code shows how to log an
event that tracks the number of bytes processed
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAStatistic.h>
...
Void myFunction(){
int instanceId = 0x1234; // change to e.g. a TaskId or some other unique ID
int numBytes= 567; // change to number of bytes actually processed
Log_write4(UIAStatistic_bytesProcessedByInstance, (IArg)__FILE__,(IArg)__LINE__,instanceId,numBytes);
}
The following text will be displayed for the event:
Bytes Processed at Line 123 in demo.c (InstanceId 0x1234): Num Bytes=567
C SYNOPSIS
| config UIAStatistic.cpuLoad // module-wide |
 |
Number of cycles used by an XDC module
| XDCscript usage |
meta-domain |
msg: "CPU Load: NumCycles=%d"
};
VALUES
numCycles
the CPU load in cycles
EXAMPLE
The following C code shows how to log a cpuLoad
event that tracks the number of cycles used by an XDC module.
The module ID is logged along with the event. For non-XDC
code, or for code with multiple instances @see #cpuLoadByInstance.
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAStatistic.h>
...
Void myFunction(){
int numCycles = 0;
// update numCycles with the number of cycles processed
Log_write1(UIAStatistic_cpuLoad, numCycles);
}
The following text will be displayed for the event:
C SYNOPSIS
| config UIAStatistic.cpuLoadByInstance // module-wide |
 |
Number of cycles used by a non XDC module or thread
| XDCscript usage |
meta-domain |
msg: "CPU Load for %s (instanceId = 0x%x): NumCycles=%d"
};
VALUES
name
a constant string that provides the name of the entity that is processing the data
instanceId
the instance ID (e.g. thread handle) of the entity that is processing the data
numCycles
the CPU load in cycles
EXAMPLE
The following C code shows how to log a cpuLoad
event that tracks the number of cycles used by
code that is not in an XDC module or by a thread
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAStatistic.h>
static volatile int gMyGlobalInstanceId = 0;
...
Void myFunction(){
IArg key;
int localInstanceId;
int numCycles = 0;
// protect pre-increment operation from race conditions
key = Gate_enterSystem();
localInstanceId = ++gMyGlobalInstanceId;
Gate_leaveSystem(key);
// update numCycles with the number of cycles processed
Log_write3(UIAStatistic_cpuLoadByInstance, "myFunction",localInstanceId,numCycles);
}
The following text will be displayed for the event:
CPU Load for myFunction (instanceId = 0x1234): NumCycles=1234
C SYNOPSIS
| config UIAStatistic.freeBytes // module-wide |
 |
Number of free bytes in heap
| XDCscript usage |
meta-domain |
msg: "Heap at %$F (HeapId 0x%x): Free Bytes=%d"
};
VALUES
__FILE__
constant string identifying the file the event was logged from
__LINE__
the line number the event was logged from
heapId
heap identifier (e.g IHeap_Handle)
freeBytes
the number of bytes free on the heap
EXAMPLE
The following C code shows how to log a freeBytes
event that tracks the number of bytes free in the heap
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAStatistic.h>
...
Void myFunction(){
int heapId = 0x1234; // change to heap ID
int numBytesFree = 567; // change to number of bytes free on the heap
Log_write4(UIAStatistic_freeBytes, (IArg)__FILE__,(IArg)__LINE__,heapId,numFreeBytes);
}
The following text will be displayed for the event:
Heap at Line 123 in demo.c (HeapId 0x1234): Free Bytes=567
C SYNOPSIS
| config UIAStatistic.wordsProcessed // module-wide |
 |
wordsProcessed statistic event
| XDCscript usage |
meta-domain |
msg: "Words Processed by %s: NumWords=0x%x"
};
VALUES
name
a constant string that provides the name
of the entity that is processing the data
numWords
the number of words processed
DETAILS
number of words that were processed.
C SYNOPSIS
| config UIAStatistic.wordsProcessedByInstance // module-wide |
 |
wordsProcessedByInstance statistic event
| XDCscript usage |
meta-domain |
msg: "Words Processed at %$F (InstanceId 0x%x): Num Words=%d"
};
VALUES
__FILE__
constant string identifying the file the event was logged from
__LINE__
the line number the event was logged from
instanceId
the instance ID (e.g. thread handle) of the
entity that is processing the data
numWords
the number of words processed
DETAILS
Number of words that were processed along with filename,
line number and instance ID.
EXAMPLE
The following C code shows how to log an
event that tracks the number of words processed
#include <xdc/runtime/Log.h>
#include <ti/uia/events/UIAStatistic.h>
...
Void myFunction(){
int instanceId = 0x1234; // change to e.g. a TaskId or some other unique ID
int numWords= 567; // change to number of words actually processed
Log_write4(UIAStatistic_wordsProcessedByInstance, (IArg)__FILE__,(IArg)__LINE__,instanceId,numWords);
}
The following text will be displayed for the event:
Words Processed at Line 123 in demo.c (InstanceId 0x1234): Num Words=567
C SYNOPSIS
| metaonly config UIAStatistic.common$ // module-wide |
 |
Common module configuration parameters
| XDCscript usage |
meta-domain |
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
generated on Wed, 26 Oct 2011 00:41:23 GMT