Inter processor communication common headers
This is a package that serves as a container for common header files
for various IPC modules supplied with the IPC product.
[
more ... ]
package ti.ipc [1, 0, 0, 0] {
}
DETAILS
This is a package that serves as a container for common header files
for various IPC modules supplied with the IPC product.
Documentation for all runtime APIs, instance configuration parameters,
error codes macros and type definitions available to the application
integrator can be found in the
Doxygen documentation
for the IPC product. However, the documentation presented in RTSC cdoc
should be referred to for information specific to the RTSC module, such as
module configuration, Errors, and Asserts.
The following table shows a list of all IPC modules that have common header
files. Follow the corresponding links for doxygen or cdoc documentation
for each of the modules.
| GateMP |
Multiple processor gate that provides local and remote context protection |
Doxygen |
cdoc |
| HeapBufMP |
Multi-processor fixed-size buffer heap |
Doxygen |
cdoc |
| HeapMemMP |
Multi-processor variable size buffer heap |
Doxygen |
cdoc |
| HeapMultiBufMP |
Multiple fixed size buffer heap |
Doxygen |
cdoc |
| Ipc |
Ipc Manager |
Doxygen |
cdoc |
| ListMP |
Multiple processor shared memory list |
Doxygen |
cdoc |
| MessageQ |
Message-passing with queuing |
Doxygen |
cdoc |
| MultiProc |
Processor id manager |
Doxygen |
cdoc |
| NameServer |
Name manager |
Doxygen |
cdoc |
| Notify |
Notification manager for IPC |
Doxygen |
cdoc |
| SharedRegion |
Shared memory manager and address translator |
Doxygen |
cdoc |
generated on Fri, 21 Aug 2015 19:35:26 GMT