module ti.ipc.family.tci6614.Interrupt

TCI6614 IPC interrupt manager

C synopsis target-domain sourced in ti/ipc/family/tci6614/Interrupt.xdc
#include <ti/ipc/family/tci6614/Interrupt.h>
Functions
UInt 
Void 
Functions common to all IInterrupt modules
UInt 
Void 
Void 
Void 
Void 
Void 
Functions common to all target modules
Defines
#define
Typedefs
typedef struct
Constants
extern const Bool 
 
 
const Interrupt_INVALIDPAYLOAD
C synopsis target-domain
#define Interrupt_INVALIDPAYLOAD (UInt)0xFFFFFFFF
 
 
struct Interrupt_IntInfo
C synopsis target-domain
typedef struct Interrupt_IntInfo {
    UInt localIntId;
    UInt remoteIntId;
    UInt intVectorId;
} Interrupt_IntInfo;
 
 
config Interrupt_enableKick  // module-wide

If set to 'true' IPC will unlock the KICK registers on C66x devices

C synopsis target-domain
extern const Bool Interrupt_enableKick;
 
DETAILS
IPC unlocks the KICK registers on the local core if (and only if) all the following conditions are met: - This configuration is set to 'true' - SharedRegion #0 is valid and the local core is its owner - SharedRegion #0 is not valid and the local core is CORE0
 
Interrupt_checkAndClear()  // module-wide

Check to see that interrupt is set, if so clear it and return 1

C synopsis target-domain
UInt Interrupt_checkAndClear(UInt16 remoteProcId, Interrupt_IntInfo *intInfo);
 
 
Interrupt_intClear()  // module-wide

Clear interrupt

C synopsis target-domain
UInt Interrupt_intClear(UInt16 remoteProcId, IInterrupt_IntInfo *intInfo);
 
ARGUMENTS
remoteProcId — Remote MultiProc Id
intInfo — Information needed to configure interrupt line
RETURNS
Value (if any) of the interrupt before it was cleared
 
Interrupt_intClearAll()  // module-wide

Clear all pending interrupts

C synopsis target-domain
Void Interrupt_intClearAll();
 
 
Interrupt_intDisable()  // module-wide

Disables the interrupt corresponding to intId

C synopsis target-domain
Void Interrupt_intDisable(UInt16 remoteProcId, IInterrupt_IntInfo *intInfo);
 
ARGUMENTS
remoteProcId — Remote MultiProc Id
intInfo — Information needed to configure interrupt line
 
Interrupt_intEnable()  // module-wide

Enables the interrupt corresponding to intId

C synopsis target-domain
Void Interrupt_intEnable(UInt16 remoteProcId, IInterrupt_IntInfo *intInfo);
 
ARGUMENTS
remoteProcId — Remote MultiProc Id
intInfo — Information needed to configure interrupt line
 
Interrupt_intRegister()  // module-wide

Register an interrupt line to a remote processor

C synopsis target-domain
Void Interrupt_intRegister(UInt16 remoteProcId, IInterrupt_IntInfo *intInfo, Fxn func, UArg arg);
 
ARGUMENTS
remoteProcId — Remote MultiProc Id
intInfo — Information needed to configure interrupt line
func — Function to register.
arg — Argument that will be passed to func
 
Interrupt_intSend()  // module-wide

Send interrupt to the remote processor

C synopsis target-domain
Void Interrupt_intSend(UInt16 remoteProcId, IInterrupt_IntInfo *intInfo, UArg arg);
 
ARGUMENTS
remoteProcId — Remote MultiProc Id
intInfo — Information needed to configure interrupt line
arg — Argument for sending interrupt.
 
Interrupt_intUnregister()  // module-wide

Unregister an interrupt line to a remote processor

C synopsis target-domain
Void Interrupt_intUnregister(UInt16 remoteProcId, IInterrupt_IntInfo *intInfo);
 
ARGUMENTS
remoteProcId — Remote MultiProc Id
intInfo — Information needed to configure interrupt line
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId Interrupt_Module_id();
// Get this module's unique id
 
Bool Interrupt_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle Interrupt_Module_heap();
// The heap from which this module allocates memory
 
Bool Interrupt_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 Interrupt_Module_getMask();
// Returns the diagnostics mask for this module
 
Void Interrupt_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
Configuration settings sourced in ti/ipc/family/tci6614/Interrupt.xdc
var Interrupt = xdc.useModule('ti.ipc.family.tci6614.Interrupt');
module-wide constants & types
    const Interrupt.INVALIDPAYLOAD//  = 0xFFFFFFFF;
 
    var obj = new Interrupt.IntInfo// ;
        obj.localIntId = UInt  ...
        obj.remoteIntId = UInt  ...
        obj.intVectorId = UInt  ...
module-wide config parameters
 
 
 
const Interrupt.INVALIDPAYLOAD
Configuration settings
const Interrupt.INVALIDPAYLOAD = 0xFFFFFFFF;
 
C SYNOPSIS
 
struct Interrupt.IntInfo
Configuration settings
var obj = new Interrupt.IntInfo;
 
    obj.localIntId = UInt  ...
    obj.remoteIntId = UInt  ...
    obj.intVectorId = UInt  ...
 
C SYNOPSIS
 
config Interrupt.enableKick  // module-wide

If set to 'true' IPC will unlock the KICK registers on C66x devices

Configuration settings
Interrupt.enableKick = Bool true;
 
DETAILS
IPC unlocks the KICK registers on the local core if (and only if) all the following conditions are met: - This configuration is set to 'true' - SharedRegion #0 is valid and the local core is its owner - SharedRegion #0 is not valid and the local core is CORE0
C SYNOPSIS
 
metaonly config Interrupt.common$  // module-wide

Common module configuration parameters

Configuration settings
Interrupt.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
generated on Fri, 21 Aug 2015 19:35:28 GMT