The transport implements a queue using a circular buffer in the manner
indicated by the following diagram.
NOTE: Processors '0' and '1' correspond to the processors with lower and
higher MultiProc ids, respectively
sharedAddr -> --------------------------- bytes
| entry0 (0) [Put] | 4
| entry1 (0) | 4
| ... |
| entryN (0) | 4
| [align to cache size] |
|-------------------------|
| putWriteIndex (0) | 4
| [align to cache size] |
|-------------------------|
| putReadIndex (0) | 4
| [align to cache size] |
|-------------------------|
| entry0 (1) [Get] | 4
| entry1 (1) | 4
| ... |
| entryN (1) | 4
| [align to cache size] |
|-------------------------|
| getWriteIndex (1) | 4
| [align to cache size] |
|-------------------------|
| getReadIndex (1) | 4
| [align to cache size] |
|-------------------------|
Legend:
(0), (1) : Memory that belongs to the proc with lower and higher
MultiProc.id, respectively
|----| : Cache line boundary
| enum TransportShmCirc_Reason |
 |
Reason for error function being called
typedef enum TransportShmCirc_Reason {
TransportShmCirc_Reason_FAILEDPUT,
TransportShmCirc_Reason_INTERNALERR,
TransportShmCirc_Reason_PHYSICALERR,
TransportShmCirc_Reason_FAILEDALLOC
} TransportShmCirc_Reason;
DETAILS
First field in the
errFxn
| enum TransportShmCirc_Status |
 |
Transport return values
typedef enum TransportShmCirc_Status {
TransportShmCirc_S_SUCCESS,
TransportShmCirc_E_FAIL,
TransportShmCirc_E_ERROR
} TransportShmCirc_Status;
DETAILS
- S_SUCCESS: Operation was successful
- E_FAIL: Operation resulted in a failure
- E_ERROR: Operation resulted in an error.
| typedef TransportShmCirc_ErrFxn |
 |
Typedef for transport error callback function
DETAILS
First parameter: Why the error function is being called.
Second parameter: Handle of transport that had the error. NULL denotes
that it is a system error, not a specific transport.
Third parameter: Pointer to the message. This is only valid for
Reason_FAILEDPUT.
Fourth parameter: Transport specific information. Refer to individual
transports for more details.
| config TransportShmCirc_enableStats // module-wide |
 |
Enable statistics for sending an event
extern const Bool TransportShmCirc_enableStats;
DETAILS
If this parameter is to 'TRUE' and 'waitClear' is also set to
TRUE when calling (@link #sendEvent(), then the module keeps
track of the number of times the processor spins waiting for
an empty slot and the max amount of time it waits.
| config TransportShmCirc_errFxn // module-wide |
 |
Asynchronous error function for the transport module
| config TransportShmCirc_notifyEventId // module-wide |
 |
Notify event ID for transport
extern const UInt16 TransportShmCirc_notifyEventId;
| config TransportShmCirc_numMsgs // module-wide |
 |
The number of messages or slots in the circular buffer
extern const UInt TransportShmCirc_numMsgs;
DETAILS
This is use to determine the size of the put and get buffers.
Each eventEntry is two 32bits wide, therefore the total size
of each circular buffer is [numMsgs * sizeof(eventEntry)].
The total size of each buffer must be a multiple of the
the cache line size. For example, if the cacheLineSize = 128
then numMsgs could be 16, 32, etc...
| TransportShmCirc_setErrFxn() // module-wide |
 |
Sets the asynchronous error function for the transport module
ARGUMENTS
errFxn
Function that is called when an asynchronous
error occurs.
DETAILS
This API allows the user to set the function that will be called in
case of an asynchronous error by the transport.
| Module-Wide Built-Ins |
 |
// Get this module's unique id
Bool TransportShmCirc_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool TransportShmCirc_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 TransportShmCirc_Module_getMask();
// Returns the diagnostics mask for this module
Void TransportShmCirc_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
| Instance Object Types |
 |
typedef struct TransportShmCirc_Object TransportShmCirc_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct TransportShmCirc_Struct TransportShmCirc_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
| Instance Config Parameters |
 |
typedef struct TransportShmCirc_Params {
// Instance config-params structure
// Common per-instance configs
UInt priority;
// Which priority messages should this transport manage
Ptr sharedAddr;
// Address in shared memory where this instance will be placed
} TransportShmCirc_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
| config TransportShmCirc_Params.priority // instance |
 |
Which priority messages should this transport manage
| config TransportShmCirc_Params.sharedAddr // instance |
 |
Address in shared memory where this instance will be placed
DETAILS
Use
sharedMemReq to determine the amount of shared memory
required.
| Runtime Instance Creation |
 |
// Allocate and initialize a new instance object and return its handle
// Initialize a new instance object inside the provided structure
ARGUMENTS
procId
Remote processor id that this instance
will communicate with.
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
This function creates a transport instance. The transport is
responsible for registering with MessageQ via the
ti.sdo.ipc.MessageQ.registerTransport API.
| Instance Deletion |
 |
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
// Finalize the instance object inside the provided structure
| TransportShmCirc_control() // instance |
 |
Send a control command to the transport instance
ARGUMENTS
handle
handle of a previously-created TransportShmCirc instance object
cmd
Requested command
cmdArgs
Accompanying field for the command. This is
command specific.
RETURNS
TRUE denotes acceptance of the command. FALSE
denotes failure of the command.
DETAILS
This is function allows transport to specify control commands. Refer
to individual transport implementions for more details.
| TransportShmCirc_getStatus() // instance |
 |
Status of a Transport instance
ARGUMENTS
handle
handle of a previously-created TransportShmCirc instance object
RETURNS
Returns status of Transport instance
DETAILS
This function returns the status of the transport instance.
| TransportShmCirc_put() // instance |
 |
Put the message to the remote processor
ARGUMENTS
handle
handle of a previously-created TransportShmCirc instance object
msg
Pointer the message to be sent
RETURNS
TRUE denotes acceptance of the message to
be sent. FALSE denotes the message could not be
sent.
DETAILS
If the transport can accept the message, it returns TRUE. Accepting
a message does not mean that it is transmitted. It simply means that
the transport should be able to send the message. If the actual transfer
fails, the transport calls the {@#ErrFxn} (assuming it is set up via the
{@#setErrFxn} API. If the {@#ErrFxn} is not set, the message is dropped.
(also...should an error be raised or just System_printf?).
If the transport cannot send the message, it returns FALSE and a
filled in Error_Block. The caller still owns the message.
| Instance Convertors |
 |
// unconditionally move one level up the inheritance hierarchy
// conditionally move one level down the inheritance hierarchy; NULL upon failure
| Instance Built-Ins |
 |
Int TransportShmCirc_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object
| enum TransportShmCirc.Reason |
 |
Reason for error function being called
values of type TransportShmCirc.Reason
const TransportShmCirc.Reason_FAILEDPUT;
const TransportShmCirc.Reason_INTERNALERR;
const TransportShmCirc.Reason_PHYSICALERR;
const TransportShmCirc.Reason_FAILEDALLOC;
DETAILS
First field in the
errFxn
C SYNOPSIS
| enum TransportShmCirc.Status |
 |
Transport return values
values of type TransportShmCirc.Status
const TransportShmCirc.S_SUCCESS;
const TransportShmCirc.E_FAIL;
const TransportShmCirc.E_ERROR;
DETAILS
- S_SUCCESS: Operation was successful
- E_FAIL: Operation resulted in a failure
- E_ERROR: Operation resulted in an error.
C SYNOPSIS
| config TransportShmCirc.enableStats // module-wide |
 |
Enable statistics for sending an event
TransportShmCirc.enableStats = Bool false;
DETAILS
If this parameter is to 'TRUE' and 'waitClear' is also set to
TRUE when calling (@link #sendEvent(), then the module keeps
track of the number of times the processor spins waiting for
an empty slot and the max amount of time it waits.
C SYNOPSIS
| config TransportShmCirc.errFxn // module-wide |
 |
Asynchronous error function for the transport module
C SYNOPSIS
| config TransportShmCirc.notifyEventId // module-wide |
 |
Notify event ID for transport
TransportShmCirc.notifyEventId = UInt16 2;
C SYNOPSIS
| config TransportShmCirc.numMsgs // module-wide |
 |
The number of messages or slots in the circular buffer
TransportShmCirc.numMsgs = UInt 32;
DETAILS
This is use to determine the size of the put and get buffers.
Each eventEntry is two 32bits wide, therefore the total size
of each circular buffer is [numMsgs * sizeof(eventEntry)].
The total size of each buffer must be a multiple of the
the cache line size. For example, if the cacheLineSize = 128
then numMsgs could be 16, 32, etc...
C SYNOPSIS
| metaonly config TransportShmCirc.common$ // module-wide |
 |
Common module configuration parameters
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
| metaonly config TransportShmCirc.rovViewInfo // module-wide |
 |
| Instance Config Parameters |
 |
var params = new TransportShmCirc.Params;
// Instance config-params object
params.priority = UInt 0;
// Which priority messages should this transport manage
params.sharedAddr = Ptr null;
// Address in shared memory where this instance will be placed
| config TransportShmCirc.Params.priority // instance |
 |
Which priority messages should this transport manage
var params = new TransportShmCirc.Params;
...
params.priority = UInt 0;
C SYNOPSIS
| config TransportShmCirc.Params.sharedAddr // instance |
 |
Address in shared memory where this instance will be placed
var params = new TransportShmCirc.Params;
...
params.sharedAddr = Ptr null;
DETAILS
Use
sharedMemReq to determine the amount of shared memory
required.
C SYNOPSIS
| Static Instance Creation |
 |
var params =
new TransportShmCirc.
Params;
// Allocate instance config-params
params.config = ...
// Assign individual configs
var inst = TransportShmCirc.create(UInt16 procId, params);
// Create an instance-object
ARGUMENTS
procId
Remote processor id that this instance
will communicate with.
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
This function creates a transport instance. The transport is
responsible for registering with MessageQ via the
ti.sdo.ipc.MessageQ.registerTransport API.