module ti.sdo.ipc.notifyDrivers.NotifySetupNull
C synopsis target-domain sourced in ti/sdo/ipc/notifyDrivers/NotifySetupNull.xdc
 
NotifySetupNull_attach()  // module-wide

Function that will be called in Notify_attach

C synopsis target-domain
Int NotifySetupNull_attach(UInt16 remoteProcId, Ptr sharedAddr);
 
 
NotifySetupNull_numIntLines()  // module-wide

Returns number of interrupt lines to the processor

C synopsis target-domain
UInt16 NotifySetupNull_numIntLines(UInt16 remoteProcId);
 
 
NotifySetupNull_sharedMemReq()  // module-wide

Shared Memory Required for a single notification line

C synopsis target-domain
SizeT NotifySetupNull_sharedMemReq(UInt16 remoteProcId, Ptr sharedAddr);
 
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId NotifySetupNull_Module_id();
// Get this module's unique id
 
Bool NotifySetupNull_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle NotifySetupNull_Module_heap();
// The heap from which this module allocates memory
 
Bool NotifySetupNull_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 NotifySetupNull_Module_getMask();
// Returns the diagnostics mask for this module
 
Void NotifySetupNull_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
Configuration settings sourced in ti/sdo/ipc/notifyDrivers/NotifySetupNull.xdc
var NotifySetupNull = xdc.useModule('ti.sdo.ipc.notifyDrivers.NotifySetupNull');
module-wide config parameters
 
 
metaonly config NotifySetupNull.common$  // module-wide

Common module configuration parameters

Configuration settings
NotifySetupNull.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
generated on Thu, 29 Jan 2015 19:16:32 GMT