module ti.sdo.ipc.gates.GateHWSem

Multiprocessor gate that utilizes hardware semaphores

C synopsis target-domain sourced in ti/sdo/ipc/gates/GateHWSem.xdc
#include <ti/sdo/ipc/gates/GateHWSem.h>
Functions
Void
Void
Void
Void
Functions common to all IGateProvider modules
Bool 
Functions common to all IGateMPSupport modules
SizeT 
Functions common to all target instances
Functions common to all target modules
Defines
#define
#define
Typedefs
typedef struct
typedef struct
typedef struct
Constants
extern const Assert_Id 
 
 
const GateHWSem_Q_BLOCKING

Blocking quality

C synopsis target-domain
#define GateHWSem_Q_BLOCKING (Int)1
 
DETAILS
Gates with this "quality" may cause the calling thread to block; i.e., suspend execution until another thread leaves the gate.
 
const GateHWSem_Q_PREEMPTING

Preempting quality

C synopsis target-domain
#define GateHWSem_Q_PREEMPTING (Int)2
 
DETAILS
Gates with this "quality" allow other threads to preempt the thread that has already entered the gate.
 
config GateHWSem_A_invSemNum  // module-wide

Asserted when supplied semNum is invalid for the relevant device

C synopsis target-domain
extern const Assert_Id GateHWSem_A_invSemNum;
 
 
GateHWSem_query()  // module-wide

Runtime test for a particular gate quality

C synopsis target-domain
Bool GateHWSem_query(Int qual);
 
ARGUMENTS
qual — constant describing a quality
RETURNS
Returns TRUE if the gate has the given quality, and FALSE otherwise, which includes the case when the gate does not recognize the constant describing the quality.
 
GateHWSem_sharedMemReq()  // module-wide

Amount of shared memory required for creation of each instance

C synopsis target-domain
SizeT GateHWSem_sharedMemReq(IGateMPSupport_Params *params);
 
ARGUMENTS
params — Pointer to the parameters that will be used in the create.
DETAILS
The value returned by this function may depend on the cache alignment requirements for the shared region from which memory will be used.
RETURNS
Number of MAUs needed to create the instance.
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId GateHWSem_Module_id();
// Get this module's unique id
 
Bool GateHWSem_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle GateHWSem_Module_heap();
// The heap from which this module allocates memory
 
Bool GateHWSem_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 GateHWSem_Module_getMask();
// Returns the diagnostics mask for this module
 
Void GateHWSem_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types

C synopsis target-domain
typedef struct GateHWSem_Object GateHWSem_Object;
// Opaque internal representation of an instance object
 
typedef GateHWSem_Object *GateHWSem_Handle;
// Client reference to an instance object
 
typedef struct GateHWSem_Struct GateHWSem_Struct;
// Opaque client structure large enough to hold an instance object
 
GateHWSem_Handle GateHWSem_handle(GateHWSem_Struct *structP);
// Convert this instance structure pointer into an instance handle
 
GateHWSem_Struct *GateHWSem_struct(GateHWSem_Handle handle);
// Convert this instance handle into an instance structure pointer
Instance Config Parameters

C synopsis target-domain
typedef struct GateHWSem_Params {
// Instance config-params structure
    IInstance_Params *instance;
    // Common per-instance configs
    UInt resourceId;
    // Logical resource id
    Ptr sharedAddr;
    // Physical address of the shared memory
} GateHWSem_Params;
 
Void GateHWSem_Params_init(GateHWSem_Params *params);
// Initialize this config-params structure with supplier-specified defaults before instance creation
 
config GateHWSem_Params.resourceId  // instance

Logical resource id

C synopsis target-domain
struct GateHWSem_Params {
      ...
    UInt resourceId;
 
 
config GateHWSem_Params.sharedAddr  // instance

Physical address of the shared memory

C synopsis target-domain
struct GateHWSem_Params {
      ...
    Ptr sharedAddr;
 
DETAILS
This parameter is only used by GateMP delegates that use shared memory
Runtime Instance Creation

C synopsis target-domain
GateHWSem_Handle GateHWSem_create(IGateProvider_Handle localGate, const GateHWSem_Params *params, Error_Block *eb);
// Allocate and initialize a new instance object and return its handle
 
Void GateHWSem_construct(GateHWSem_Struct *structP, IGateProvider_Handle localGate, const GateHWSem_Params *params);
// Initialize a new instance object inside the provided structure
ARGUMENTS
localGate — Gate to use for local protection.
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Non-NULL gate for local protection must be passed to the create call. If no local protection is desired, a xdc.runtime.GateNull handle must be passed in.
Instance Deletion

C synopsis target-domain
Void GateHWSem_delete(GateHWSem_Handle *handleP);
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
 
Void GateHWSem_destruct(GateHWSem_Struct *structP);
// Finalize the instance object inside the provided structure
Instance Convertors

C synopsis target-domain
IGateMPSupport_Handle GateHWSem_Handle_upCast(GateHWSem_Handle handle);
// unconditionally move one level up the inheritance hierarchy
 
GateHWSem_Handle GateHWSem_Handle_downCast(IGateMPSupport_Handle handle);
// conditionally move one level down the inheritance hierarchy; NULL upon failure
 
IGateProvider_Handle GateHWSem_Handle_upCast2(GateHWSem_Handle handle);
// unconditionally move 2 levels up the inheritance hierarchy
 
GateHWSem_Handle GateHWSem_Handle_downCast2(IGateProvider_Handle handle);
// conditionally move 2 levels down the inheritance hierarchy; NULL upon failure
Instance Built-Ins

C synopsis target-domain
Int GateHWSem_Object_count();
// The number of statically-created instance objects
 
GateHWSem_Handle GateHWSem_Object_get(GateHWSem_Object *array, Int i);
// The handle of the i-th statically-created instance object (array == NULL)
 
GateHWSem_Handle GateHWSem_Object_first();
// The handle of the first dynamically-created instance object, or NULL
 
GateHWSem_Handle GateHWSem_Object_next(GateHWSem_Handle handle);
// The handle of the next dynamically-created instance object, or NULL
 
IHeap_Handle GateHWSem_Object_heap();
// The heap used to allocate dynamically-created instance objects
 
Types_Label *GateHWSem_Handle_label(GateHWSem_Handle handle, Types_Label *buf);
// The label associated with this instance object
 
String GateHWSem_Handle_name(GateHWSem_Handle handle);
// The name of this instance object
 
Configuration settings sourced in ti/sdo/ipc/gates/GateHWSem.xdc
var GateHWSem = xdc.useModule('ti.sdo.ipc.gates.GateHWSem');
module-wide constants & types
module-wide config parameters
        msg: "A_invSemNum: Invalid hardware semaphore number"
    };
 
module-wide functions
per-instance config parameters
    var params = new GateHWSem.Params// Instance config-params object;
        params.resourceId// Logical resource id = UInt 0;
        params.sharedAddr// Physical address of the shared memory = Ptr null;
per-instance creation
    var inst = GateHWSem.create// Create an instance-object(IGateProvider.Handle localGate, params);
 
 
const GateHWSem.Q_BLOCKING

Blocking quality

Configuration settings
const GateHWSem.Q_BLOCKING = 1;
 
DETAILS
Gates with this "quality" may cause the calling thread to block; i.e., suspend execution until another thread leaves the gate.
C SYNOPSIS
 
const GateHWSem.Q_PREEMPTING

Preempting quality

Configuration settings
const GateHWSem.Q_PREEMPTING = 2;
 
DETAILS
Gates with this "quality" allow other threads to preempt the thread that has already entered the gate.
C SYNOPSIS
 
config GateHWSem.A_invSemNum  // module-wide

Asserted when supplied semNum is invalid for the relevant device

Configuration settings
GateHWSem.A_invSemNum = Assert.Desc {
    msg: "A_invSemNum: Invalid hardware semaphore number"
};
 
C SYNOPSIS
 
metaonly config GateHWSem.common$  // module-wide

Common module configuration parameters

Configuration settings
GateHWSem.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
 
metaonly GateHWSem.getNumResources()  // module-wide

Returns the number of resources offered by the GateMP delegate

Configuration settings
GateHWSem.getNumResources() returns UInt
 
 
metaonly GateHWSem.queryMeta()  // module-wide

Configuration time test for a particular gate quality

Configuration settings
GateHWSem.queryMeta(Int qual) returns Bool
 
ARGUMENTS
qual — constant describing a quality
RETURNS
Returns TRUE if the gate has the given quality, and FALSE otherwise, which includes the case when the gate does not recognize the constant describing the quality.
 
metaonly GateHWSem.setReserved()  // module-wide

Reserve a HW sempahore for use outside of IPC

Configuration settings
GateHWSem.setReserved(UInt semNum) returns Void
 
ARGUMENTS
semNum — HW semaphore number to reserve
DETAILS
GateMP will, by default, manage all HW semaphores on the device unless this API is used to set aside specific HW semaphores for use outside of IPC.
Instance Config Parameters

Configuration settings
var params = new GateHWSem.Params;
// Instance config-params object
    params.resourceId = UInt 0;
    // Logical resource id
    params.sharedAddr = Ptr null;
    // Physical address of the shared memory
 
config GateHWSem.Params.resourceId  // instance

Logical resource id

Configuration settings
var params = new GateHWSem.Params;
  ...
params.resourceId = UInt 0;
 
C SYNOPSIS
 
config GateHWSem.Params.sharedAddr  // instance

Physical address of the shared memory

Configuration settings
var params = new GateHWSem.Params;
  ...
params.sharedAddr = Ptr null;
 
DETAILS
This parameter is only used by GateMP delegates that use shared memory
C SYNOPSIS
Static Instance Creation

Configuration settings
var params = new GateHWSem.Params;
// Allocate instance config-params
params.config =   ...
// Assign individual configs
 
var inst = GateHWSem.create(IGateProvider.Handle localGate, params);
// Create an instance-object
ARGUMENTS
localGate — Gate to use for local protection.
params — per-instance config params, or NULL to select default values (target-domain only)
eb — active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Non-NULL gate for local protection must be passed to the create call. If no local protection is desired, a xdc.runtime.GateNull handle must be passed in.
generated on Thu, 29 Jan 2015 19:16:27 GMT