module ti.sdo.ipc.family.ti81xx.NotifyMbxSetup

Notify setup proxy for NotifyDriverMbx on TI81XX

This module creates and registers all drivers necessary for inter-processor notifications using ti.sdo.ipc.family.ti81xx.NotifyDriverMbxmore ... ]
C synopsis target-domain sourced in ti/sdo/ipc/family/ti81xx/NotifyMbxSetup.xdc
DETAILS
This module creates and registers all drivers necessary for inter-processor notifications using ti.sdo.ipc.family.ti81xx.NotifyDriverMbx
Configure the dspIntVectId module config to choose a non-default interrupt vector ID on the TI81XX DSP core.
 
config NotifyMbxSetup_dspIntVectId  // module-wide

Interrupt vector id for the DSP core on TI81XX

C synopsis target-domain
extern const UInt NotifyMbxSetup_dspIntVectId;
 
 
NotifyMbxSetup_attach()  // module-wide

Function that will be called in Notify_attach

C synopsis target-domain
Int NotifyMbxSetup_attach(UInt16 remoteProcId, Ptr sharedAddr);
 
 
NotifyMbxSetup_numIntLines()  // module-wide

Returns number of interrupt lines to the processor

C synopsis target-domain
UInt16 NotifyMbxSetup_numIntLines(UInt16 remoteProcId);
 
 
NotifyMbxSetup_sharedMemReq()  // module-wide

Shared Memory Required for a single notification line

C synopsis target-domain
SizeT NotifyMbxSetup_sharedMemReq(UInt16 remoteProcId, Ptr sharedAddr);
 
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId NotifyMbxSetup_Module_id();
// Get this module's unique id
 
Bool NotifyMbxSetup_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle NotifyMbxSetup_Module_heap();
// The heap from which this module allocates memory
 
Bool NotifyMbxSetup_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 NotifyMbxSetup_Module_getMask();
// Returns the diagnostics mask for this module
 
Void NotifyMbxSetup_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
Configuration settings sourced in ti/sdo/ipc/family/ti81xx/NotifyMbxSetup.xdc
var NotifyMbxSetup = xdc.useModule('ti.sdo.ipc.family.ti81xx.NotifyMbxSetup');
module-wide config parameters
 
 
 
config NotifyMbxSetup.dspIntVectId  // module-wide

Interrupt vector id for the DSP core on TI81XX

Configuration settings
NotifyMbxSetup.dspIntVectId = UInt 5;
 
C SYNOPSIS
 
metaonly config NotifyMbxSetup.common$  // module-wide

Common module configuration parameters

Configuration settings
NotifyMbxSetup.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
generated on Thu, 29 Jan 2015 19:16:40 GMT