Creates the default notify drivers for each pair of processors.
| enum NotifySetup_ARM_INT |
 |
Possible incoming interrupt IDs for DaVinci/ARM
typedef enum NotifySetup_ARM_INT {
NotifySetup_ARM_INT0,
NotifySetup_ARM_INT1
} NotifySetup_ARM_INT;
| enum NotifySetup_DSP_INT |
 |
Possible incoming interrupt IDs for DaVinci/DSP
typedef enum NotifySetup_DSP_INT {
NotifySetup_DSP_INT0,
NotifySetup_DSP_INT1,
NotifySetup_DSP_INT2,
NotifySetup_DSP_INT3
} NotifySetup_DSP_INT;
| config NotifySetup_armRecvIntId0 // module-wide |
 |
Incoming interrupt ID for line #0 line on ARM
extern const UInt NotifySetup_armRecvIntId0;
DETAILS
See
ARM_INT for possible values.
| config NotifySetup_armRecvIntId1 // module-wide |
 |
Incoming interrupt ID for line #1 line on ARM
extern const UInt NotifySetup_armRecvIntId1;
DETAILS
See
ARM_INT for possible values.
| config NotifySetup_dspIntVectId0 // module-wide |
 |
Vector ID to use on DSP for line #0
extern const UInt NotifySetup_dspIntVectId0;
| config NotifySetup_dspIntVectId1 // module-wide |
 |
Vector ID to use on DSP for line #1
extern const UInt NotifySetup_dspIntVectId1;
| config NotifySetup_dspRecvIntId0 // module-wide |
 |
Incoming interrupt ID for line #0 line on DSP
extern const UInt NotifySetup_dspRecvIntId0;
DETAILS
See
DSP_INT for possible values.
| config NotifySetup_dspRecvIntId1 // module-wide |
 |
Incoming interrupt ID for line #1 line on DSP
extern const UInt NotifySetup_dspRecvIntId1;
DETAILS
See
DSP_INT for possible values.
| config NotifySetup_useSecondLine // module-wide |
 |
Enable the second interrupt line on DaVinci
extern const Bool NotifySetup_useSecondLine;
| NotifySetup_attach() // module-wide |
 |
Function that will be called in Notify_attach
Int NotifySetup_attach(UInt16 remoteProcId, Ptr sharedAddr);
| NotifySetup_numIntLines() // module-wide |
 |
Returns number of interrupt lines to the processor
UInt16 NotifySetup_numIntLines(UInt16 remoteProcId);
| NotifySetup_sharedMemReq() // module-wide |
 |
Shared Memory Required for a single notification line
SizeT NotifySetup_sharedMemReq(UInt16 remoteProcId, Ptr sharedAddr);
| Module-Wide Built-Ins |
 |
// Get this module's unique id
Bool NotifySetup_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool NotifySetup_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 NotifySetup_Module_getMask();
// Returns the diagnostics mask for this module
Void NotifySetup_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module