module ti.sdo.ipc.family.dm6446.NotifyCircSetup

Manages setup of the default Notify driver handles

Creates the default notify drivers for each pair of processors.
C synopsis target-domain sourced in ti/sdo/ipc/family/dm6446/NotifyCircSetup.xdc
#include <ti/sdo/ipc/family/dm6446/NotifyCircSetup.h>
Functions common to all INotifySetup modules
Int 
UInt16 
SizeT 
Functions common to all target modules
Typedefs
typedef enum
typedef enum
Constants
extern const UInt 
extern const UInt 
extern const UInt 
extern const UInt 
extern const UInt 
extern const UInt 
extern const Bool 
 
 
enum NotifyCircSetup_ARM_INT

Possible incoming interrupt IDs for DaVinci/ARM

C synopsis target-domain
typedef enum NotifyCircSetup_ARM_INT {
    NotifyCircSetup_ARM_INT0,
    NotifyCircSetup_ARM_INT1
} NotifyCircSetup_ARM_INT;
 
 
enum NotifyCircSetup_DSP_INT

Possible incoming interrupt IDs for DaVinci/DSP

C synopsis target-domain
typedef enum NotifyCircSetup_DSP_INT {
    NotifyCircSetup_DSP_INT0,
    NotifyCircSetup_DSP_INT1,
    NotifyCircSetup_DSP_INT2,
    NotifyCircSetup_DSP_INT3
} NotifyCircSetup_DSP_INT;
 
 
config NotifyCircSetup_armRecvIntId0  // module-wide

Incoming interrupt ID for line #0 line on ARM

C synopsis target-domain
extern const UInt NotifyCircSetup_armRecvIntId0;
 
DETAILS
See ARM_INT for possible values.
 
config NotifyCircSetup_armRecvIntId1  // module-wide

Incoming interrupt ID for line #1 line on ARM

C synopsis target-domain
extern const UInt NotifyCircSetup_armRecvIntId1;
 
DETAILS
See ARM_INT for possible values.
 
config NotifyCircSetup_dspIntVectId0  // module-wide

Vector ID to use on DSP for line #0

C synopsis target-domain
extern const UInt NotifyCircSetup_dspIntVectId0;
 
 
config NotifyCircSetup_dspIntVectId1  // module-wide

Vector ID to use on DSP for line #1

C synopsis target-domain
extern const UInt NotifyCircSetup_dspIntVectId1;
 
 
config NotifyCircSetup_dspRecvIntId0  // module-wide

Incoming interrupt ID for line #0 line on DSP

C synopsis target-domain
extern const UInt NotifyCircSetup_dspRecvIntId0;
 
DETAILS
See DSP_INT for possible values.
 
config NotifyCircSetup_dspRecvIntId1  // module-wide

Incoming interrupt ID for line #1 line on DSP

C synopsis target-domain
extern const UInt NotifyCircSetup_dspRecvIntId1;
 
DETAILS
See DSP_INT for possible values.
 
config NotifyCircSetup_useSecondLine  // module-wide

Enable the second interrupt line on DaVinci

C synopsis target-domain
extern const Bool NotifyCircSetup_useSecondLine;
 
 
NotifyCircSetup_attach()  // module-wide

Function that will be called in Notify_attach

C synopsis target-domain
Int NotifyCircSetup_attach(UInt16 remoteProcId, Ptr sharedAddr);
 
 
NotifyCircSetup_numIntLines()  // module-wide

Returns number of interrupt lines to the processor

C synopsis target-domain
UInt16 NotifyCircSetup_numIntLines(UInt16 remoteProcId);
 
 
NotifyCircSetup_sharedMemReq()  // module-wide

Shared Memory Required for a single notification line

C synopsis target-domain
SizeT NotifyCircSetup_sharedMemReq(UInt16 remoteProcId, Ptr sharedAddr);
 
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId NotifyCircSetup_Module_id();
// Get this module's unique id
 
Bool NotifyCircSetup_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle NotifyCircSetup_Module_heap();
// The heap from which this module allocates memory
 
Bool NotifyCircSetup_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 NotifyCircSetup_Module_getMask();
// Returns the diagnostics mask for this module
 
Void NotifyCircSetup_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
Configuration settings sourced in ti/sdo/ipc/family/dm6446/NotifyCircSetup.xdc
 
enum NotifyCircSetup.ARM_INT

Possible incoming interrupt IDs for DaVinci/ARM

Configuration settings
values of type NotifyCircSetup.ARM_INT
    const NotifyCircSetup.ARM_INT0;
    const NotifyCircSetup.ARM_INT1;
 
C SYNOPSIS
 
enum NotifyCircSetup.DSP_INT

Possible incoming interrupt IDs for DaVinci/DSP

Configuration settings
values of type NotifyCircSetup.DSP_INT
    const NotifyCircSetup.DSP_INT0;
    const NotifyCircSetup.DSP_INT1;
    const NotifyCircSetup.DSP_INT2;
    const NotifyCircSetup.DSP_INT3;
 
C SYNOPSIS
 
config NotifyCircSetup.armRecvIntId0  // module-wide

Incoming interrupt ID for line #0 line on ARM

Configuration settings
NotifyCircSetup.armRecvIntId0 = UInt NotifyCircSetup.ARM_INT0;
 
DETAILS
See ARM_INT for possible values.
C SYNOPSIS
 
config NotifyCircSetup.armRecvIntId1  // module-wide

Incoming interrupt ID for line #1 line on ARM

Configuration settings
NotifyCircSetup.armRecvIntId1 = UInt NotifyCircSetup.ARM_INT1;
 
DETAILS
See ARM_INT for possible values.
C SYNOPSIS
 
config NotifyCircSetup.dspIntVectId0  // module-wide

Vector ID to use on DSP for line #0

Configuration settings
NotifyCircSetup.dspIntVectId0 = UInt 5;
 
C SYNOPSIS
 
config NotifyCircSetup.dspIntVectId1  // module-wide

Vector ID to use on DSP for line #1

Configuration settings
NotifyCircSetup.dspIntVectId1 = UInt 6;
 
C SYNOPSIS
 
config NotifyCircSetup.dspRecvIntId0  // module-wide

Incoming interrupt ID for line #0 line on DSP

Configuration settings
NotifyCircSetup.dspRecvIntId0 = UInt NotifyCircSetup.DSP_INT0;
 
DETAILS
See DSP_INT for possible values.
C SYNOPSIS
 
config NotifyCircSetup.dspRecvIntId1  // module-wide

Incoming interrupt ID for line #1 line on DSP

Configuration settings
NotifyCircSetup.dspRecvIntId1 = UInt NotifyCircSetup.DSP_INT1;
 
DETAILS
See DSP_INT for possible values.
C SYNOPSIS
 
config NotifyCircSetup.useSecondLine  // module-wide

Enable the second interrupt line on DaVinci

Configuration settings
NotifyCircSetup.useSecondLine = Bool false;
 
C SYNOPSIS
 
metaonly config NotifyCircSetup.common$  // module-wide

Common module configuration parameters

Configuration settings
NotifyCircSetup.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
generated on Thu, 29 Jan 2015 19:16:42 GMT