Creates the default notify drivers for each pair of processors.
| enum NotifyCircSetup_ARM_INT |
 |
Possible incoming interrupt IDs for ARM
typedef enum NotifyCircSetup_ARM_INT {
NotifyCircSetup_ARM_INT0,
NotifyCircSetup_ARM_INT1
} NotifyCircSetup_ARM_INT;
| enum NotifyCircSetup_DSP_INT |
 |
Possible incoming interrupt IDs for DSP
typedef enum NotifyCircSetup_DSP_INT {
NotifyCircSetup_DSP_INT0,
NotifyCircSetup_DSP_INT1
} NotifyCircSetup_DSP_INT;
| config NotifyCircSetup_armRecvIntId0 // module-wide |
 |
Incoming interrupt ID for line #0 line on ARM
extern const UInt NotifyCircSetup_armRecvIntId0;
DETAILS
See
ARM_INT for possible values.
| config NotifyCircSetup_armRecvIntId1 // module-wide |
 |
Incoming interrupt ID for line #1 line on ARM
extern const UInt NotifyCircSetup_armRecvIntId1;
DETAILS
See
ARM_INT for possible values.
| config NotifyCircSetup_dspIntVectId0 // module-wide |
 |
Vector ID to use on DSP for line #1
extern const UInt NotifyCircSetup_dspIntVectId0;
| config NotifyCircSetup_dspIntVectId1 // module-wide |
 |
Vector ID to use on DSP for line #1
extern const UInt NotifyCircSetup_dspIntVectId1;
| config NotifyCircSetup_dspRecvIntId0 // module-wide |
 |
Incoming interrupt ID for line #0 line on DSP
extern const UInt NotifyCircSetup_dspRecvIntId0;
DETAILS
See
DSP_INT for possible values.
| config NotifyCircSetup_dspRecvIntId1 // module-wide |
 |
Incoming interrupt ID for line #1 line on DSP
extern const UInt NotifyCircSetup_dspRecvIntId1;
DETAILS
See
DSP_INT for possible values.
| config NotifyCircSetup_useSecondLine // module-wide |
 |
Enable the second interrupt line
extern const Bool NotifyCircSetup_useSecondLine;
| NotifyCircSetup_attach() // module-wide |
 |
Function that will be called in Notify_attach
Int NotifyCircSetup_attach(UInt16 remoteProcId, Ptr sharedAddr);
| NotifyCircSetup_numIntLines() // module-wide |
 |
Returns number of interrupt lines to the processor
UInt16 NotifyCircSetup_numIntLines(UInt16 remoteProcId);
| NotifyCircSetup_sharedMemReq() // module-wide |
 |
Shared Memory Required for a single notification line
SizeT NotifyCircSetup_sharedMemReq(UInt16 remoteProcId, Ptr sharedAddr);
| Module-Wide Built-Ins |
 |
// Get this module's unique id
Bool NotifyCircSetup_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool NotifyCircSetup_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 NotifyCircSetup_Module_getMask();
// Returns the diagnostics mask for this module
Void NotifyCircSetup_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module