| const GateHWSem_Q_BLOCKING |
 |
Blocking quality
#define GateHWSem_Q_BLOCKING (Int)1
DETAILS
Gates with this "quality" may cause the calling thread to block;
i.e., suspend execution until another thread leaves the gate.
| const GateHWSem_Q_PREEMPTING |
 |
Preempting quality
#define GateHWSem_Q_PREEMPTING (Int)2
DETAILS
Gates with this "quality" allow other threads to preempt the thread
that has already entered the gate.
| config GateHWSem_A_invSemNum // module-wide |
 |
Asserted when supplied semNum is invalid for the relevant device
extern const Assert_Id GateHWSem_A_invSemNum;
| GateHWSem_query() // module-wide |
 |
Runtime test for a particular gate quality
Bool GateHWSem_query(Int qual);
ARGUMENTS
qual
constant describing a quality
RETURNS
Returns TRUE if the gate has the given quality,
and FALSE otherwise, which includes the case when the gate does not
recognize the constant describing the quality.
| GateHWSem_sharedMemReq() // module-wide |
 |
Amount of shared memory required for creation of each instance
ARGUMENTS
params
Pointer to the parameters that will be used in
the create.
DETAILS
The value returned by this function may depend on the cache alignment
requirements for the shared region from which memory will be used.
RETURNS
Number of MAUs needed to create the instance.
| Module-Wide Built-Ins |
 |
// Get this module's unique id
Bool GateHWSem_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool GateHWSem_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 GateHWSem_Module_getMask();
// Returns the diagnostics mask for this module
Void GateHWSem_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
| Instance Object Types |
 |
typedef struct GateHWSem_Object GateHWSem_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct GateHWSem_Struct GateHWSem_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
| Instance Config Parameters |
 |
typedef struct GateHWSem_Params {
// Instance config-params structure
// Common per-instance configs
UInt resourceId;
// Logical resource id
Ptr sharedAddr;
// Physical address of the shared memory
} GateHWSem_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
| config GateHWSem_resourceId // instance |
 |
Logical resource id
| config GateHWSem_sharedAddr // instance |
 |
Physical address of the shared memory
DETAILS
This parameter is only used by GateMP delegates that use shared memory
| Instance Creation |
 |
// Allocate and initialize a new instance object and return its handle
// Initialize a new instance object inside the provided structure
ARGUMENTS
localGate
Gate to use for local protection.
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Non-NULL gate for local protection must be passed to the create
call. If no local protection is desired, a
xdc.runtime.GateNull handle must be passed in.
| Instance Deletion |
 |
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
// Finalize the instance object inside the provided structure
| Instance Convertors |
 |
// unconditionally move one level up the inheritance hierarchy
// conditionally move one level down the inheritance hierarchy; NULL upon failure
// unconditionally move 2 levels up the inheritance hierarchy
// conditionally move 2 levels down the inheritance hierarchy; NULL upon failure
| Instance Built-Ins |
 |
Int GateHWSem_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object
| const GateHWSem.Q_BLOCKING |
 |
Blocking quality
| XDCscript usage |
meta-domain |
const GateHWSem.Q_BLOCKING = 1;
DETAILS
Gates with this "quality" may cause the calling thread to block;
i.e., suspend execution until another thread leaves the gate.
C SYNOPSIS
| const GateHWSem.Q_PREEMPTING |
 |
Preempting quality
| XDCscript usage |
meta-domain |
const GateHWSem.Q_PREEMPTING = 2;
DETAILS
Gates with this "quality" allow other threads to preempt the thread
that has already entered the gate.
C SYNOPSIS
| config GateHWSem.A_invSemNum // module-wide |
 |
Asserted when supplied semNum is invalid for the relevant device
| XDCscript usage |
meta-domain |
msg: "A_invSemNum: Invalid hardware semaphore number"
};
C SYNOPSIS
| metaonly config GateHWSem.common$ // module-wide |
 |
Common module configuration parameters
| XDCscript usage |
meta-domain |
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
| metaonly GateHWSem.getNumResources() // module-wide |
 |
Returns the number of resources offered by the GateMP delegate
| XDCscript usage |
meta-domain |
GateHWSem.getNumResources() returns UInt
| metaonly GateHWSem.queryMeta() // module-wide |
 |
Configuration time test for a particular gate quality
| XDCscript usage |
meta-domain |
GateHWSem.queryMeta(Int qual) returns Bool
ARGUMENTS
qual
constant describing a quality
RETURNS
Returns TRUE if the gate has the given quality,
and FALSE otherwise, which includes the case when the gate does not
recognize the constant describing the quality.
| metaonly GateHWSem.setReserved() // module-wide |
 |
Reserve a HW sempahore for use outside of IPC
| XDCscript usage |
meta-domain |
GateHWSem.setReserved(UInt semNum) returns Void
ARGUMENTS
semNum
HW semaphore number to reserve
DETAILS
GateMP will, by default, manage all HW semaphores on the device unless
this API is used to set aside specific HW semaphores for use outside
of IPC.
| Instance Config Parameters |
 |
| XDCscript usage |
meta-domain |
var params = new GateHWSem.Params;
// Instance config-params object
params.resourceId = UInt 0;
// Logical resource id
params.sharedAddr = Ptr null;
// Physical address of the shared memory
| config GateHWSem.resourceId // instance |
 |
Logical resource id
| XDCscript usage |
meta-domain |
var params = new GateHWSem.Params;
...
params.resourceId = UInt 0;
C SYNOPSIS
| config GateHWSem.sharedAddr // instance |
 |
Physical address of the shared memory
| XDCscript usage |
meta-domain |
var params = new GateHWSem.Params;
...
params.sharedAddr = Ptr null;
DETAILS
This parameter is only used by GateMP delegates that use shared memory
C SYNOPSIS
| Instance Creation |
 |
| XDCscript usage |
meta-domain |
var params =
new GateHWSem.
Params;
// Allocate instance config-params
params.config = ...
// Assign individual configs
// Create an instance-object
ARGUMENTS
localGate
Gate to use for local protection.
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Non-NULL gate for local protection must be passed to the create
call. If no local protection is desired, a
xdc.runtime.GateNull handle must be passed in.