module ti.sdo.ipc.family.da830.NotifySetup

Manages setup of the default Notify driver handles

Creates the default notify drivers for each pair of processors.
C synopsis target-domain sourced in ti/sdo/ipc/family/da830/NotifySetup.xdc
#include <ti/sdo/ipc/family/da830/NotifySetup.h>
Functions common to all INotifySetup modules
Int 
UInt16 
SizeT 
Functions common to all target modules
Typedefs
typedef enum
typedef enum
Constants
extern const UInt 
extern const UInt 
extern const UInt 
extern const UInt 
extern const UInt 
extern const UInt 
extern const Bool 
 
 
enum NotifySetup_ARM_INT

Possible incoming interrupt IDs for ARM

C synopsis target-domain
typedef enum NotifySetup_ARM_INT {
    NotifySetup_ARM_INT0,
    NotifySetup_ARM_INT1
} NotifySetup_ARM_INT;
 
 
enum NotifySetup_DSP_INT

Possible incoming interrupt IDs for DSP

C synopsis target-domain
typedef enum NotifySetup_DSP_INT {
    NotifySetup_DSP_INT0,
    NotifySetup_DSP_INT1
} NotifySetup_DSP_INT;
 
 
config NotifySetup_armRecvIntId0  // module-wide

Incoming interrupt ID for line #0 line on ARM

C synopsis target-domain
extern const UInt NotifySetup_armRecvIntId0;
 
DETAILS
See ARM_INT for possible values.
 
config NotifySetup_armRecvIntId1  // module-wide

Incoming interrupt ID for line #1 line on ARM

C synopsis target-domain
extern const UInt NotifySetup_armRecvIntId1;
 
DETAILS
See ARM_INT for possible values.
 
config NotifySetup_dspIntVectId0  // module-wide

Vector ID to use on DSP for line #0

C synopsis target-domain
extern const UInt NotifySetup_dspIntVectId0;
 
 
config NotifySetup_dspIntVectId1  // module-wide

Vector ID to use on DSP for line #1

C synopsis target-domain
extern const UInt NotifySetup_dspIntVectId1;
 
 
config NotifySetup_dspRecvIntId0  // module-wide

Incoming interrupt ID for line #0 line on DSP

C synopsis target-domain
extern const UInt NotifySetup_dspRecvIntId0;
 
DETAILS
See DSP_INT for possible values.
 
config NotifySetup_dspRecvIntId1  // module-wide

Incoming interrupt ID for line #1 line on DSP

C synopsis target-domain
extern const UInt NotifySetup_dspRecvIntId1;
 
DETAILS
See DSP_INT for possible values.
 
config NotifySetup_useSecondLine  // module-wide

Enable the second interrupt line

C synopsis target-domain
extern const Bool NotifySetup_useSecondLine;
 
 
NotifySetup_attach()  // module-wide

Function that will be called in Notify_attach

C synopsis target-domain
Int NotifySetup_attach(UInt16 remoteProcId, Ptr sharedAddr);
 
 
NotifySetup_numIntLines()  // module-wide

Returns number of interrupt lines to the processor

C synopsis target-domain
UInt16 NotifySetup_numIntLines(UInt16 remoteProcId);
 
 
NotifySetup_sharedMemReq()  // module-wide

Shared Memory Required for a single notification line

C synopsis target-domain
SizeT NotifySetup_sharedMemReq(UInt16 remoteProcId, Ptr sharedAddr);
 
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId NotifySetup_Module_id();
// Get this module's unique id
 
Bool NotifySetup_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle NotifySetup_Module_heap();
// The heap from which this module allocates memory
 
Bool NotifySetup_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 NotifySetup_Module_getMask();
// Returns the diagnostics mask for this module
 
Void NotifySetup_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
XDCscript usage meta-domain sourced in ti/sdo/ipc/family/da830/NotifySetup.xdc
 
enum NotifySetup.ARM_INT

Possible incoming interrupt IDs for ARM

XDCscript usage meta-domain
values of type NotifySetup.ARM_INT
    const NotifySetup.ARM_INT0;
    const NotifySetup.ARM_INT1;
 
C SYNOPSIS
 
enum NotifySetup.DSP_INT

Possible incoming interrupt IDs for DSP

XDCscript usage meta-domain
values of type NotifySetup.DSP_INT
    const NotifySetup.DSP_INT0;
    const NotifySetup.DSP_INT1;
 
C SYNOPSIS
 
config NotifySetup.armRecvIntId0  // module-wide

Incoming interrupt ID for line #0 line on ARM

XDCscript usage meta-domain
NotifySetup.armRecvIntId0 = UInt NotifySetup.ARM_INT0;
 
DETAILS
See ARM_INT for possible values.
C SYNOPSIS
 
config NotifySetup.armRecvIntId1  // module-wide

Incoming interrupt ID for line #1 line on ARM

XDCscript usage meta-domain
NotifySetup.armRecvIntId1 = UInt NotifySetup.ARM_INT1;
 
DETAILS
See ARM_INT for possible values.
C SYNOPSIS
 
config NotifySetup.dspIntVectId0  // module-wide

Vector ID to use on DSP for line #0

XDCscript usage meta-domain
NotifySetup.dspIntVectId0 = UInt 5;
 
C SYNOPSIS
 
config NotifySetup.dspIntVectId1  // module-wide

Vector ID to use on DSP for line #1

XDCscript usage meta-domain
NotifySetup.dspIntVectId1 = UInt 6;
 
C SYNOPSIS
 
config NotifySetup.dspRecvIntId0  // module-wide

Incoming interrupt ID for line #0 line on DSP

XDCscript usage meta-domain
NotifySetup.dspRecvIntId0 = UInt NotifySetup.DSP_INT0;
 
DETAILS
See DSP_INT for possible values.
C SYNOPSIS
 
config NotifySetup.dspRecvIntId1  // module-wide

Incoming interrupt ID for line #1 line on DSP

XDCscript usage meta-domain
NotifySetup.dspRecvIntId1 = UInt NotifySetup.DSP_INT1;
 
DETAILS
See DSP_INT for possible values.
C SYNOPSIS
 
config NotifySetup.useSecondLine  // module-wide

Enable the second interrupt line

XDCscript usage meta-domain
NotifySetup.useSecondLine = Bool false;
 
C SYNOPSIS
 
metaonly config NotifySetup.common$  // module-wide

Common module configuration parameters

XDCscript usage meta-domain
NotifySetup.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
generated on Wed, 19 Oct 2011 18:03:58 GMT