module ti.sdo.ipc.family.arctic.NotifySetup

Notify setup proxy for ARP32

This module creates and registers all drivers necessary for inter-processor notification on ARP32.
C synopsis target-domain sourced in ti/sdo/ipc/family/arctic/NotifySetup.xdc
 
config NotifySetup_dspIntVectId  // module-wide

Interrupt vector id for ARP32/DSP

C synopsis target-domain
extern const UInt NotifySetup_dspIntVectId;
 
 
NotifySetup_attach()  // module-wide

Function that will be called in Notify_attach

C synopsis target-domain
Int NotifySetup_attach(UInt16 remoteProcId, Ptr sharedAddr);
 
 
NotifySetup_numIntLines()  // module-wide

Returns number of interrupt lines to the processor

C synopsis target-domain
UInt16 NotifySetup_numIntLines(UInt16 remoteProcId);
 
 
NotifySetup_sharedMemReq()  // module-wide

Shared Memory Required for a single notification line

C synopsis target-domain
SizeT NotifySetup_sharedMemReq(UInt16 remoteProcId, Ptr sharedAddr);
 
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId NotifySetup_Module_id();
// Get this module's unique id
 
Bool NotifySetup_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle NotifySetup_Module_heap();
// The heap from which this module allocates memory
 
Bool NotifySetup_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 NotifySetup_Module_getMask();
// Returns the diagnostics mask for this module
 
Void NotifySetup_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
XDCscript usage meta-domain sourced in ti/sdo/ipc/family/arctic/NotifySetup.xdc
var NotifySetup = xdc.useModule('ti.sdo.ipc.family.arctic.NotifySetup');
module-wide config parameters
 
 
 
config NotifySetup.dspIntVectId  // module-wide

Interrupt vector id for ARP32/DSP

XDCscript usage meta-domain
NotifySetup.dspIntVectId = UInt 4;
 
C SYNOPSIS
 
metaonly config NotifySetup.common$  // module-wide

Common module configuration parameters

XDCscript usage meta-domain
NotifySetup.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
generated on Wed, 19 Oct 2011 18:03:54 GMT