interface xdc.runtime.knl.ISync

OS independent synchronization

This interface allows clients to select method of synchronization in an OS independent way. [ more ... ]
XDCspec summary sourced in xdc/runtime/knl/ISync.xdc
interface ISync {  ...
// inherits xdc.runtime.IModule
instance:  ...
XDCspec declarations sourced in xdc/runtime/knl/ISync.xdc
package xdc.runtime.knl;
 
interface ISync {
module-wide constants & types
    const UInt NO_WAIT// Used to specify no waiting = 0;
    const Int Q_BLOCKING// Blocking quality = 1;
    const UInt WAIT_FOREVER// Used to wait forever = ~(0);
 
        WaitStatus_ERROR,
        WaitStatus_TIMEOUT,
        WaitStatus_SUCCESS
    };
module-wide config parameters
 
 
instance:
per-instance creation
per-instance functions
    Bool query// Query for a particular quality(Int qual);
}
DETAILS
This interface allows clients to select method of synchronization in an OS independent way.
Modules that require the user to pick a synchronization method, will request a Handle. Clients of such modules can pick a blocking ISync implementation or a non-blocking implementation.
This interface specifies two main functions signal and wait. These two functions are always used in pairs in modules that use ISync instances. The signal() function is used to signal completion of an activity. The wait() function will allow the module to block or poll for completion of the same activity.
ISync mandates that the sync mechanism be binary and not support counters. Although the wait() function seems meaningless in the case of non-blocking sync, it allows modules to be written generically and support all ISync implementations. For non-blocking ISync the wait() function will return WaitStatus_TIMEOUT to denote timeout.
 
const ISync.NO_WAIT

Used to specify no waiting

XDCspec declarations sourced in xdc/runtime/knl/ISync.xdc
const UInt NO_WAIT = 0;
 
 
const ISync.Q_BLOCKING

Blocking quality

XDCspec declarations sourced in xdc/runtime/knl/ISync.xdc
const Int Q_BLOCKING = 1;
 
DETAILS
Implementations with this "quality" may cause the calling thread to block;
 
const ISync.WAIT_FOREVER

Used to wait forever

XDCspec declarations sourced in xdc/runtime/knl/ISync.xdc
const UInt WAIT_FOREVER = ~(0);
 
 
enum ISync.WaitStatus

Error codes returned by ISync_wait

XDCspec declarations sourced in xdc/runtime/knl/ISync.xdc
enum WaitStatus {
    WaitStatus_ERROR,
    WaitStatus_TIMEOUT,
    WaitStatus_SUCCESS
};
 
 
metaonly config ISync.common$  // module-wide

Common module configuration parameters

XDCspec declarations sourced in xdc/runtime/knl/ISync.xdc
metaonly config Types.Common$ common$;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
Instance Creation

XDCspec declarations sourced in xdc/runtime/knl/ISync.xdc
create();
// Create an instance-object
 
ISync.query()  // instance

Query for a particular quality

XDCspec declarations sourced in xdc/runtime/knl/ISync.xdc
Bool query(Int qual);
 
ARGUMENTS
qual — quality
RETURNS
TRUE or FALSE.
DETAILS
FALSE is returned if quality not supported.
 
ISync.signal()  // instance

Called at completion of an activity

XDCspec declarations sourced in xdc/runtime/knl/ISync.xdc
Void signal();
 
DETAILS
This function is non-blocking. It is also required that the underlying sync be binary in nature.
This function does not take an Error.Block intentionally because it can be called from ISR context.
 
ISync.wait()  // instance

Called to wait/poll for completion of an activity

XDCspec declarations sourced in xdc/runtime/knl/ISync.xdc
Int wait(UInt timeout, Error.Block *eb);
 
ARGUMENTS
timeout — Timeout in microseconds
eb — Hist Pointer to Error.Block
RETURNS
Refer to description above
DETAILS
This function can block. Non-blocking implementations should return WaitStatus_TIMEOUT to indicate a timeout.
generated on Sat, 11 Feb 2012 01:20:03 GMT